Member's Forum Vacuum Fluorescent Display Help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 634 subscribers
  • Views 1972 views
  • Users 0 members are here
  • interfacing
  • hardware
  • vacuum_fluorescent_display
  • vfd
Related

Vacuum Fluorescent Display Help

blast
blast over 13 years ago

Hi,

I've been given a 16 character, 14 segment (plus decimal point & comma tail) starburst Vacuum Fluorescent Display, which was recovered from a fruit machine 20 odd years ago, and would like to get going again; connecting it to either a PC or Raspberry Pi.

 

The VFD board is mounted on a driver board via headers, the VFD circuit is labelled 'Barcrest 682225 19364-2', while the driver board is labelled '15178-3' & '101 D/IC' - Barcrest is a fruit machine manufacturer in the UK.

 

I've attached a photo of the device.

 

The driver board has 5 wires (White, Yellow, Orange, Black & Red).

The driver board contains one 40 Pin Dual In-Line package, which is labelled:

'Rockwell

10937P-40

A8201-30

MEXICO

9313 A30133-4'

 

I've looked this up online and found a datasheet (attached PDF) for what appears to be a copy made under license, and have derived the following connections for the wires:

White - SLCK (Clock)

Yellow - Data

Orange - Reset Maybe?

Black - Negative DC voltage?

Red - Positive DC Voltage?

 

Any idea what kind of voltage/ current requirements this device may have (PDF datasheet seems to suggest 15v is typical)?  I'm hoping that before going too far, I can power it up and see the display initialise to ensure it actually works.  After that I'd like to get it connected (via serial?) to a PC or Raspberry Pi so I can send text to it, are there any guides for showing how to connect VFDs up/ send data etc, as I don't really know where to start.

 

Thanks in advance!

Attachments:
image
imagedatasheet.pdf
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    Hi blast,

    It's a nice-looking display. On it's own, the glass requires some unusual voltages compared to (say) LED displays; basically, the IC requires 15V (or a +5V and -10V supply, which will still provide a total of 15V across it), but the VFD may require a lower voltage than that. However, there is a possibility that the power supplies (to step-down - and step-up if needed) are integrated on the board, so that you could power from (say) +5V or some other voltage, and use normal 5V  logic levels to control it (it won't work with 3.3V logic levels according to the datasheet you supplied). Look for a small wound transformer on-board as a clue in case it has an on-board supply. You'll need a power supply capable of a few hundred milliamps.

    To get to 3.3V logic levels you'd need to use a level converter (google for some information on that). You'd have to toggle bits using an RPI or something, this is not a standard PC interface.

    So, in summary it is possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 13 years ago

    Hi blast,

    It's a nice-looking display. On it's own, the glass requires some unusual voltages compared to (say) LED displays; basically, the IC requires 15V (or a +5V and -10V supply, which will still provide a total of 15V across it), but the VFD may require a lower voltage than that. However, there is a possibility that the power supplies (to step-down - and step-up if needed) are integrated on the board, so that you could power from (say) +5V or some other voltage, and use normal 5V  logic levels to control it (it won't work with 3.3V logic levels according to the datasheet you supplied). Look for a small wound transformer on-board as a clue in case it has an on-board supply. You'll need a power supply capable of a few hundred milliamps.

    To get to 3.3V logic levels you'd need to use a level converter (google for some information on that). You'd have to toggle bits using an RPI or something, this is not a standard PC interface.

    So, in summary it is possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • blast
    0 blast over 13 years ago in reply to shabaz

    Hi Shabaz, thanks for you reply.

    You're right, the driver board does contain a coil.  I've attached another photo - you can see it in the middle of the board.

    So I guess my best bet is to give it 5v and see if it lights up (I'm assuming it will flash all segments as part of a self test), if nothing happens then increase the voltage torward 15v.