• Products and Partners
    Products and Partners
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
Member's Forum What "MICROCONTROLLER" that is best for IMAGE PROCESSING?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 632 subscribers
  • Views 2822 views
  • Users 0 members are here
Related

What "MICROCONTROLLER" that is best for IMAGE PROCESSING?

e14 Contributor
e14 Contributor over 12 years ago

I am a senior computer engineering student from the Philippines, and One of my module of my project is an IMAGE PROCESSING waste segregation where it segregates
trashes by "biodegradable" or "non-biodegradable". I hope that you could help me guys.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    missing a key component and im sure you all know this

     

    Speed of analysis

     

    If this is a conveyor then the system must analyse in almost real-time, yes there is a lag but it must be able to keep up with the conveyor, this will require a very fast processing sub system or many small systems working on concert

     

    all the other points are perfectly valid also, we just need to add the dimension of performance, this in itself would probably eliminate things like PI, BBB etc. From a proof of concept they will work but for production it would need to be massively scaled up, or the conveyor slowed down image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    missing a key component and im sure you all know this

     

    Speed of analysis

     

    If this is a conveyor then the system must analyse in almost real-time, yes there is a lag but it must be able to keep up with the conveyor, this will require a very fast processing sub system or many small systems working on concert

     

    all the other points are perfectly valid also, we just need to add the dimension of performance, this in itself would probably eliminate things like PI, BBB etc. From a proof of concept they will work but for production it would need to be massively scaled up, or the conveyor slowed down image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Peter Oakes wrote:

     

    missing a key component and im sure you all know this

     

    Speed of analysis

     

    If this is a conveyor then the system must analyse in almost real-time, yes there is a lag but it must be able to keep up with the conveyor, this will require a very fast processing sub system or many small systems working on concert

     

    all the other points are perfectly valid also, we just need to add the dimension of performance, this in itself would probably eliminate things like PI, BBB etc. From a proof of concept they will work but for production it would need to be massively scaled up, or the conveyor slowed down

    Im not using a conveyor.  im going to make a two trashbins: 1 for the Biodegradable and 1 for the Recyclable.
    on the top of the trashbin there is a CAMERA for image processing. If ever the person trying to put the "PLASTIC BOTTLE" to the biodegradable bin, the biodegradable bin won't open.
    If the person put the plastic on the Recyclable bin the bin will open.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer