Member's Forum Seeking info on a good adaptor that would facilitate 2 x female vga to 1 x male hdmi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 631 subscribers
  • Views 1986 views
  • Users 0 members are here
Related

Seeking info on a good adaptor that would facilitate 2 x female vga to 1 x male hdmi

Valeriem
Valeriem over 4 years ago

HI all,

Not sure if I am in the right place but I would love a recommendation on what product to use for the above. I have two monitors with male VGA connectors and my laptop only has one hdmi connector. Would anyone know if there be a cheap enough adaptor that I could access here in Ireland that would allow me to hook up both monitors to my laptop?

P.s. I have checked that the graphics card on my laptop and my OS Windows 10 can support 3 monitors.

Any help that you could give would be appreciated!!

MANY thanks, Valerie

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 4 years ago

    Hi,

    A single HDMI to multi-VGA is not a likely popular enough product to be available for such use - it's a bit too specific for your scenario.

    Amazon has USB to VGA converters however, and a couple of those could be used, but the quality is likely to be poor and low-res.

    It may be better all-round to sell the monitors and replace with a single large high-res monitor with the connector your laptop supports.

    Your laptop may allow the in-built display and the external display to be usable. There are laptop stands that support propping up at an angle, and then you can use an external keyboard.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 4 years ago

    Hi,

    A single HDMI to multi-VGA is not a likely popular enough product to be available for such use - it's a bit too specific for your scenario.

    Amazon has USB to VGA converters however, and a couple of those could be used, but the quality is likely to be poor and low-res.

    It may be better all-round to sell the monitors and replace with a single large high-res monitor with the connector your laptop supports.

    Your laptop may allow the in-built display and the external display to be usable. There are laptop stands that support propping up at an angle, and then you can use an external keyboard.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • cstanton
    0 cstanton over 4 years ago in reply to shabaz

    Agreed, talking as a person who's used a VGA to HDMI adapter, the frequency it operates at ends up being... wrong, and misaligned because you're translating from a digital to an analogue signal or vice versa.

    Sometimes they also need to be 'active' devices, so you have to connect them up to a USB power source for them to work. It's sub-optimal and not really worth messing around with, they can also end up costing more than a pair of new monitors that can accept DVI or HDMI anyway.

    Plus... I think the person's asking for HDMI to 2x VGA, which I don't believe HDMI supports - DisplayPort would be do-able, if the graphics chip supported it, with some kinda frankenstein converter to go from DisplayPort -> 2x DisplayPort -> Maybe to HDMI first -> Some downscaler device -> VGA, but you're going to need twice the hardware and a lot of adapter cables and then... just why?

    • Cancel
    • Vote Up +3 Vote Down