• Products and Partners
    Products and Partners
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
Member's Forum CREE 4FLOW LED Light Bulb Failure
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 630 subscribers
  • Views 893 views
  • Users 0 members are here
Related

CREE 4FLOW LED Light Bulb Failure

scottiebabe
scottiebabe over 4 years ago

7 Years later, this Cree 4FLOW LED light bulb finally gave up the ghost.

Based on my limited failure analysis thus far, the only failure I can see thus far is 1 of 8 cree SMD LED modules. 

The large electrolytic capacitor charges up to 300 V, when powered off a 30V bench power supply.

I thought the mechanical design of this light bulb was very innovative for its time.

image

Ultimately this bulb style never caught on. I don't know that it performs any better or last any longer than the sealed round globe bulbs.

Here are a few teardown photos:

image

image

image

image

image

Update: It Works!

I removed the dead LED module and replaced it with a 10 Ohm 0805 resistor to compete the LED string and so I can measure the LED drive current.

image

Let there be light!

image

Each LED module appears to have 10 individual LEDs

image

I powered the bulb with two power supplies in series totaling 81V and measured an operating current of 95 mA. Pin = 7.70 W

The drive voltage to the LED string was measured at 202V with a string current of 33.5 mA, Pout = 6.77 W

So for this test the efficiency was 88%, reasonable enough.

The first time I reassembled the bulb nothing happened. I had the second PCB inserted in the wrong orientation. Its a shame they didn't arrange the PCB spring contacts such that you can only make electrical contact when the PCB is inserted in the correct orientation.

  

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    scottiebabe over 4 years ago

    I don't know if it was manufactured like this but, the solder blob where the spring terminal of the second PCB contacts the main PCB has a depression in it. I'm not sure if the Bulb runs so hot that the solder is soft, or it was manufactured that way, interesting!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 4 years ago

    I don't know if it was manufactured like this but, the solder blob where the spring terminal of the second PCB contacts the main PCB has a depression in it. I'm not sure if the Bulb runs so hot that the solder is soft, or it was manufactured that way, interesting!