Member's Forum Should Handheld multimeters have color LCD displays?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 75 replies
  • Subscribers 590 subscribers
  • Views 11308 views
  • Users 0 members are here
Related

Should Handheld multimeters have color LCD displays?

scottiebabe
scottiebabe over 3 years ago

As I am waiting for my OWON HDS242 to come in the mail, I thought I might ask other members how they feel about a handheld multimeter having a power hungry color LCD display.

The product webpage suggests a battery life of 3-6 hours. https://www.owon.com.hk/products_owon_hds200_series_digital_oscilloscope 

Even more interesting/exciting is the batteries can be recharged with a USB-C cable.

Based on Kerry Wong's teardown: http://www.kerrywong.com/2021/09/18/teardown-of-an-owon-hds272s-3-in-1-handheld-oscilloscope-dmm-awg-compared-with-hantek-2d72/ the multimeter functionality is galvanically isolated from the usb connector.

What do you think?

First time trying the poll feature, hopefully I didn't goof it!

Based on Kerry's notes the meter also has the bones of a real oscilloscope (ADC, FPGA, Sample memory, etc..) How performant is oscilloscope it? I don't know yet.... But I am intrigued!

Update: The scopemeter arrived!

Indoors the color LCD looks awesome! For me my multimeter ends up either sitting flat on my desk on in my lap and in both those cases the display is 10x easier to read than a segment LCD without a backlight.

Outdoors with direct sunlight the segment LCD is easier to read than the color LCD.

In the shade outdoors, I think both display technologies are equally legible.

image

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +6
    So.... I'd say, "yes," but, I'd rather have a higher-quality monochrome than a lower-quality color. That said if I can slightly flex, a company called Kaitweets sent me one of their meters. These are…
  • Jan Cumps
    Jan Cumps over 3 years ago +4
    I voted Yes! although I don't know why I'd need it yet. In other instruments, colour has often been a gimmick in the beginning. But then real good use was found for it. I put my money on this: "in a…
  • dang74
    dang74 over 3 years ago +4
    I voted yes, but it was in context to the additional information that was provided, namely that in this case it's perfectly acceptable because the product also doubles as an oscilloscope. Should all manufacturers…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    .... and from  a LabVIEW test flow:

    image

    Yay!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    This is awesome! Great work, I would much rather use the ni-visa interface over python... I will have to look into this! I didn't know you could do raw usb over visa

    Thanks for sharing Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    Now that I've used a similar device for some time, I can answer the question with some authority Slight smile:
    Q: "Should Handheld multimeters have color LCD displays?"
    A: "Yes. They can put better focus on different data points at the same time. It's not just a gimmick, if done well."

    (also:
    Q: "Should a DMM have the user interface firmware that this Owon's DMM module has?" 
    A: "No."
    )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago

    What if... it had two displays, and one was e-ink/e-paper?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to cstanton

    I would go for a screen capture e-ink second display.  Other than that... I'd pass.  I can barely remember to turn off the peak hold feature on my current meter - much less something with the persistence of an e-ink display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to cstanton

    A meter that turns on once per second to take reading and display it on e-ink.......could last a long time on a battery..Thumbsup tone2

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to dougw

    I'm not sure if I agree.

    After waiting for the 2nd or 3rd reading, I bet I could throw it against the wall hard enough it wouldn't last long.. regardless of the battery.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to baldengineer

    JoyJoyJoy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Hattifnatten
    Hattifnatten over 1 year ago in reply to Jan Cumps

    Hi Jan

    how did you get ni-Max to find it?

    br

    jørgen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Hattifnatten

    I don't recall it. Let me try to see if I had set up an alias, or if it found it automatically. Hang on ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>