Member's Forum Trying out a low-cost USB Microscope
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 631 subscribers
  • Views 18723 views
  • Users 0 members are here
Related

Trying out a low-cost USB Microscope

scottiebabe
scottiebabe over 3 years ago

Recently I purchased the “8 Dollar Microscope” and of course I ended up spending far more than $8… In total I ended up spending $50 CAD LOL

If you haven’t seen the microscope in discussion it is the following:

image

It is essentially 0.3 MP UVC USB webcam with optics that provide a magnification of 50x to 500x. As you can see from the product photo, the included base shown in that photo would have poor utility for looking at electronics straight down. However, I received my microscope with a plastic adjustable stand similar to the following:

image

Nice surprise! But, the included plastic stand was not easy to use, and would frequently bind up trying to adjust the height.

Assuming I would receive that tiny plastic swivel base I opted to purchase an aluminum alloy universal microscope stand:

image

The height adjustment mechanism on this stand is smooth and easy to use. There is a small amount of backlash that is noticeable when trying to focus at the highest magnification, but it isn’t severe enough for me to be bothered by it. I really like the stand I’m glad I bought it.

The USB microscope sits inside the 1.4″ mounting hole and is held in place with 2 set screws:

image

The aluminum stand looks great! The microscope doesn’t sit normal to the viewing surface, but as will be seen in the sample images it didn’t seem to be a big deal.

When the microscope was adjusted for a magnification of 50x the resulting field of view had a width of 12 mm across :

image

That is a little bit smaller than I’d like but it is what it is. I would have like to capture maybe say 50 mm across, but I would also like more image resolution…

Here are some random photos I took:

image
image
image

image
image
image

image

image
image

At maximum magnification, the lens casts a shadow onto your viewing area. So, you need to provided external lighting in that case.

Could you solder with it? At 50x magnification the working height was approximately 7cm. I think that is a personal question whether you are comfortable looking at a display and making fine movements with your hands..

Be careful with product specifications! There are 100’s of different listing for this style of usb microscope and some claim resolutions of up to 2 MP (I am skeptical that is true).

Was it a good purchase? The stand absolutely great, the microscope is fine for what it is a 0.3MP usb microscope…

The price of the digital microscopes with included displays is not that much more.

image

Of course if you have any advise or recommendations on what to look for in these 4″ or 7″ digital microscopes I would be grateful to hear it Slight smile

  • Sign in to reply
  • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to baldengineer

    yes, and rubbing just a little olive oil on the paper, makes more light go through - while keeping the diffusor effect.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to rsjawale24

    (White) paper works well sometimes too.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago in reply to shabaz

    Yup! I know the LEDs are causing the problem... I was going to post about it here and ask for suggestions. Thanks for this. I'll try to put something on the LEDs to smoothen the light, maybe a ring made of frosted acrylic sheet or just a frosted sticky tape.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to rsjawale24

    Hi!

    The camera might be ok, maybe it's just the lighting. There are reflections of each LED off the ring-light you're using, they are appearing as white reflected spots.

    It could be better to replace that with a light or two from the sides (as with the cute gooseneck LEDs on the photo from baldengineer  microscope. The shallower the angle, eventually it gets called "dark field illumination". This would also help with the second photo for instance, where the FTDI part marking is currently difficult to see. With the sideways lighting, it can be extremely clear. Another option is wider diameter ring light (that's what I use for 99% of all my photos, mainly because it's a simple single-light solution) but for a microscope it could be impractical since it would need a lot more desk space. Or, you could try to diffuse the LEDs, and dim them slightly, but then there's a good chance the image will be noisy. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago in reply to scottiebabe

    I clicked a few pictures.... The properties tab for these pictures show that the resolution is 1280 X 720, but it does not look like HD quality. I'll do a detailed write up about the scope in a few weeks. 

    image

    image

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to scottiebabe

    Agreed, I have plans for a Pi zero 2W camera as well - with auto focus.

    My microscope HQ Cam now sports a MIPI-to-USB converter, turning it into a webcam - no boot time.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to scottiebabe

    It's just flux. Clean it off and it'll look like new!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to rsjawale24

    That is exciting! This looks like one of the 4" display models. There are so many different models its hard to know which to choose!

    No rush of course, but if you ever get the chance I would be interested to see a few sample PCB photos Slight smile

    Nice microscope!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    The photos from your RPI powered microscope are absolutely wonderful!

    If the pi zero 2w ever comes back into stock, its a project I will serious consider experimenting with

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Andrew J

    LOL isn't e14 the Instagram of PCB photos? Everything looks better than in real-life. Of course after surgery my feather doesn't look so pretty!

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
>