Member's Forum Trying out a low-cost USB Microscope
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 631 subscribers
  • Views 19034 views
  • Users 0 members are here
Related

Trying out a low-cost USB Microscope

scottiebabe
scottiebabe over 3 years ago

Recently I purchased the “8 Dollar Microscope” and of course I ended up spending far more than $8… In total I ended up spending $50 CAD LOL

If you haven’t seen the microscope in discussion it is the following:

image

It is essentially 0.3 MP UVC USB webcam with optics that provide a magnification of 50x to 500x. As you can see from the product photo, the included base shown in that photo would have poor utility for looking at electronics straight down. However, I received my microscope with a plastic adjustable stand similar to the following:

image

Nice surprise! But, the included plastic stand was not easy to use, and would frequently bind up trying to adjust the height.

Assuming I would receive that tiny plastic swivel base I opted to purchase an aluminum alloy universal microscope stand:

image

The height adjustment mechanism on this stand is smooth and easy to use. There is a small amount of backlash that is noticeable when trying to focus at the highest magnification, but it isn’t severe enough for me to be bothered by it. I really like the stand I’m glad I bought it.

The USB microscope sits inside the 1.4″ mounting hole and is held in place with 2 set screws:

image

The aluminum stand looks great! The microscope doesn’t sit normal to the viewing surface, but as will be seen in the sample images it didn’t seem to be a big deal.

When the microscope was adjusted for a magnification of 50x the resulting field of view had a width of 12 mm across :

image

That is a little bit smaller than I’d like but it is what it is. I would have like to capture maybe say 50 mm across, but I would also like more image resolution…

Here are some random photos I took:

image
image
image

image
image
image

image

image
image

At maximum magnification, the lens casts a shadow onto your viewing area. So, you need to provided external lighting in that case.

Could you solder with it? At 50x magnification the working height was approximately 7cm. I think that is a personal question whether you are comfortable looking at a display and making fine movements with your hands..

Be careful with product specifications! There are 100’s of different listing for this style of usb microscope and some claim resolutions of up to 2 MP (I am skeptical that is true).

Was it a good purchase? The stand absolutely great, the microscope is fine for what it is a 0.3MP usb microscope…

The price of the digital microscopes with included displays is not that much more.

image

Of course if you have any advise or recommendations on what to look for in these 4″ or 7″ digital microscopes I would be grateful to hear it Slight smile

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 3 years ago

    I bought a unit a couple of years ago after careful examination of specifications to get the most real resolution. It works as the specs indicate, but the focus and zoom adjust are very touchy and not smooth. The stand (like the one you have) helps with adjustment although the depth of focus is miniscule. It is crucial to find a unit where the display has enough pixels to see what the camera is capturing and be sure to read the fine print that the camera resolution is not some interpolated hi-res spec. Just because the display is bigger, doesn't mean it has more pixels. I was hoping to alleviate the fatigue of using a stereo microscope, but there image quality cannot compare to a stereo microscope, so I wasn't using it at all. Eventually I built a much better system based on a R Pi HQ cam, (and I recently upgraded it to eliminate the R Pi boot time) but I still use the stereo microscope far more often. I only use the digital microscopes when I need to capture an image.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    I bought a unit a couple of years ago after careful examination of specifications to get the most real resolution. It works as the specs indicate, but the focus and zoom adjust are very touchy and not smooth. The stand (like the one you have) helps with adjustment although the depth of focus is miniscule. It is crucial to find a unit where the display has enough pixels to see what the camera is capturing and be sure to read the fine print that the camera resolution is not some interpolated hi-res spec. Just because the display is bigger, doesn't mean it has more pixels. I was hoping to alleviate the fatigue of using a stereo microscope, but there image quality cannot compare to a stereo microscope, so I wasn't using it at all. Eventually I built a much better system based on a R Pi HQ cam, (and I recently upgraded it to eliminate the R Pi boot time) but I still use the stereo microscope far more often. I only use the digital microscopes when I need to capture an image.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Children
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    The photos from your RPI powered microscope are absolutely wonderful!

    If the pi zero 2w ever comes back into stock, its a project I will serious consider experimenting with