Member's Forum Trying out a low-cost USB Microscope
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 631 subscribers
  • Views 18906 views
  • Users 0 members are here
Related

Trying out a low-cost USB Microscope

scottiebabe
scottiebabe over 3 years ago

Recently I purchased the “8 Dollar Microscope” and of course I ended up spending far more than $8… In total I ended up spending $50 CAD LOL

If you haven’t seen the microscope in discussion it is the following:

image

It is essentially 0.3 MP UVC USB webcam with optics that provide a magnification of 50x to 500x. As you can see from the product photo, the included base shown in that photo would have poor utility for looking at electronics straight down. However, I received my microscope with a plastic adjustable stand similar to the following:

image

Nice surprise! But, the included plastic stand was not easy to use, and would frequently bind up trying to adjust the height.

Assuming I would receive that tiny plastic swivel base I opted to purchase an aluminum alloy universal microscope stand:

image

The height adjustment mechanism on this stand is smooth and easy to use. There is a small amount of backlash that is noticeable when trying to focus at the highest magnification, but it isn’t severe enough for me to be bothered by it. I really like the stand I’m glad I bought it.

The USB microscope sits inside the 1.4″ mounting hole and is held in place with 2 set screws:

image

The aluminum stand looks great! The microscope doesn’t sit normal to the viewing surface, but as will be seen in the sample images it didn’t seem to be a big deal.

When the microscope was adjusted for a magnification of 50x the resulting field of view had a width of 12 mm across :

image

That is a little bit smaller than I’d like but it is what it is. I would have like to capture maybe say 50 mm across, but I would also like more image resolution…

Here are some random photos I took:

image
image
image

image
image
image

image

image
image

At maximum magnification, the lens casts a shadow onto your viewing area. So, you need to provided external lighting in that case.

Could you solder with it? At 50x magnification the working height was approximately 7cm. I think that is a personal question whether you are comfortable looking at a display and making fine movements with your hands..

Be careful with product specifications! There are 100’s of different listing for this style of usb microscope and some claim resolutions of up to 2 MP (I am skeptical that is true).

Was it a good purchase? The stand absolutely great, the microscope is fine for what it is a 0.3MP usb microscope…

The price of the digital microscopes with included displays is not that much more.

image

Of course if you have any advise or recommendations on what to look for in these 4″ or 7″ digital microscopes I would be grateful to hear it Slight smile

  • Sign in to reply
  • Cancel
  • baldengineer
    baldengineer over 3 years ago

    I have one of these with the LCD screen and (mostly) love it after two years of countless uses.

    image

    I paid about $100 for it on Amazon. It was this 7-inch that claims 12 MP. Although, it is clear there are many other models/brands that are OEMs of one design.

    The LCD's latency is low enough for soldering. The built-in battery makes for a great portable unit too. (Although, I had to refresh its 18650 to get it to hold a charge.) The additional goose neck lights REALLY help improve image quality. (As with all small sensor cameras, the more light you can provide, the lower their ISO, so the lower the noise.)

    Seriously, I cannot impress how important it is to get MOAR LIGHTS pointed at your board! You need 5 not 4 lights, in this case.

    These also have a USB port to connect to a PC. HOWEVER. You cannot use the screen and the PC connection at the same time. Which is a real bummer. Because I enjoy using OBS (or VLC) to open it as a camera on a larger screen. (or, for WBW videos and live streaming, to share the video, like in the low temp solder paste episode.). But, then the LCD is disabled. It becomes awkward to use for soldering--especially with the USB delay. (I have started to get used to it though.)

    BUT! It is FANTASTIC for inspection, especially as a standalone battery-powered unit. Whether you are checking solder joints or reading marks on an IC or looking at the balls inside of solder paste. :)

    t5 vs t3 solder balls in solder paste

    Basically, when connected to a PC, it becomes the same one scottiebabe is using except with a big awkward rectangle on top!

    Regardless, I also recommend any of these USB microscopes (with sufficiently good sensor!)

    This $100 was the best I have spent on a test tool in years.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago

    Thanks for sharing your purchase foray.

    I have had similar experience making one purchase and having to augment it with another purchase to make it work. As my teeth have gotten longer, I tend to suffer analysis paralysis trying to avoid the multiple purchases. Experience of others surely helps in avoiding the scenario.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago
    scottiebabe said:
    Be careful with product specifications! There are 100’s of different listing for this style of usb microscope and some claim resolutions of up to 2 MP (I am skeptical that is true).

    Some claim 5Mpix Slight smile

    USB Microscope - 5MP interpolated 220x magnification / 8 LEDs
    https://www.adafruit.com/product/636

    There appear to be several clones of that microscope with varying prices and image quality.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Surprisingly good images! I wonder if you were lucky, and got a unit that is well-assembled with the lenses. Very neat that you have the adjustable zoom too.

    I had expected them to not be good for the low price. Having said that, I really like the low-price Carson magnifiers etc too, and they make nice gifts for children too. For instance this type of thing for longer-distance viewing, but it can be used a foot away from an item; my 9-year old nephew loves it, and takes it everywhere.

    image

    Another source for stereo microscope could be just ebay, keeping an eye out. I got a quite decent Meiji microscope for about £100 and the guy dropped it off to my home for that price too! It was really dusty, but after 30 mins of cleaning up it was great. However if you want to get the image onto the computer then the price goes up rapidly, since you'll need the camera and adapter to drop into one of the eyepiece ports. Although it comes in handy, I rarely use the microscope day-to-day. For soldering and quick visual inspection, I use a head magnifier (OptiVISOR is great, but I have not tried other head magnifiers). I went through a lot of non-head magnifiers however, to finally realize that the head magnifier suited my needs during soldering.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 3 years ago

    The magnification looks pretty good.  I will be on the lookout for one of the models that includes the display.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago

    I went for the 3D Printed stand route.

    image


    Where'd you get the stand you're using? It looks nicely sturdy.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 3 years ago

    Those USB microscopes are great for what they are. I also find they're a good present for neices and nephews, etc.

    Personally, I think it's really worth the step up to a stereo microscope - especially if you think you'll be using it for soldering. Amscope seem to be the brand to go for in the US. In the UK they were hard to get so I went for something similar from China via eBay. I did a quick review here quite a few years ago.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
<