Member's Forum A Soldering Iron for Christmas
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 629 subscribers
  • Views 5115 views
  • Users 0 members are here
Related

A Soldering Iron for Christmas

scottiebabe
scottiebabe over 3 years ago

With a few words of encouragement from shabaz and baldengineer I snuck this bad girl into the Christmas tree!

 image

A USB-c powered portable soldering iron!

 image image

image

image

image

image

image

Fully assembled it has a similar form factor to my weller wxmp

image

With the temperature set at 300 degC it struggled a little to melt leaded solder on a copper clad board.

 

When I adjusted the temp to 330 degC the same temp I use on my weller wxmp, Id say its thermal performance felt similar (no scientific evidence).

 

The only obvious criticism I have thus far is the included silicone USB cable is a little on the short side. If the cable was 30 cm longer, I think it would be long enough. I am hopping to find a powerbank that will power this iron, at which point the USB cable length would not be an issue.

 

It also didn’t include a travel or storage pouch…

 image

But that is also okay, I think I am going to try and put together an electronics first aid kit (I have the soldering iron covered).

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    scottiebabe over 3 years ago

    There is also the "Pinecil" which is a usb-c powered soldering iron which appears to retail for $35 USD

    image

    https://pine64.com/product/pinecil-smart-mini-portable-soldering-iron/ 

    But I don't know where you would buy it or if it is any good (perhaps this is what shabaz bought)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 3 years ago

    There is also the "Pinecil" which is a usb-c powered soldering iron which appears to retail for $35 USD

    image

    https://pine64.com/product/pinecil-smart-mini-portable-soldering-iron/ 

    But I don't know where you would buy it or if it is any good (perhaps this is what shabaz bought)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    Interesting! Its 144 MHz RISC-V chip should hopefully be able to handle the soldering element heater algorithm : ) Awesome that there is so much choice, USB-C adoption for portable soldering is really high it seems.

    I went for these two, although I probably would have considered the PINECIL had I known about it:

    This one, Sequre S60, accepts JBC C210 series tips, which cover a range of surface-mount and through-hole prototyping, but are no good for large connectors:

    image

    I also ordered this "Smart Electric Soldering Iron" which looks very basic, it is pretty cheap. I don't expect it to be amazing at this price, but I was still curious if it could function as a basic soldering iron. This one is compatible with C245 series tips, which are fine for large connectors, as well as surface-mount. 

    image

    A benefit for these two models though, is that because I already have C210 and C245 tips and know what they solder like, it could be interesting to compare.