Member's Forum A Soldering Iron for Christmas
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 629 subscribers
  • Views 5109 views
  • Users 0 members are here
Related

A Soldering Iron for Christmas

scottiebabe
scottiebabe over 3 years ago

With a few words of encouragement from shabaz and baldengineer I snuck this bad girl into the Christmas tree!

 image

A USB-c powered portable soldering iron!

 image image

image

image

image

image

image

Fully assembled it has a similar form factor to my weller wxmp

image

With the temperature set at 300 degC it struggled a little to melt leaded solder on a copper clad board.

 

When I adjusted the temp to 330 degC the same temp I use on my weller wxmp, Id say its thermal performance felt similar (no scientific evidence).

 

The only obvious criticism I have thus far is the included silicone USB cable is a little on the short side. If the cable was 30 cm longer, I think it would be long enough. I am hopping to find a powerbank that will power this iron, at which point the USB cable length would not be an issue.

 

It also didn’t include a travel or storage pouch…

 image

But that is also okay, I think I am going to try and put together an electronics first aid kit (I have the soldering iron covered).

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    scottiebabe over 3 years ago

    If one was proficient in the mechanical side of things, you could DIY your own USB soldering iron (others have). I just tried heating up one of my weller tips which like the TS80P use a 3.5 mm TRS jack.

      image

    It only needed about 2.6W (2.35V @ 1.1A) to get the tip to a temperature where solder melts.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to scottiebabe
    scottiebabe said:
    I just tried heating up one of my weller tips which like the TS80P use a 3.5 mm TRS jack.

    Just don't mistake them for your ear buds... 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to beacon_dave

    usb powered heated q-tips! Heart eyes lol

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 3 years ago in reply to beacon_dave

    usb powered heated q-tips! Heart eyes lol