Member's Forum A Soldering Iron for Christmas
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 629 subscribers
  • Views 5103 views
  • Users 0 members are here
Related

A Soldering Iron for Christmas

scottiebabe
scottiebabe over 3 years ago

With a few words of encouragement from shabaz and baldengineer I snuck this bad girl into the Christmas tree!

 image

A USB-c powered portable soldering iron!

 image image

image

image

image

image

image

Fully assembled it has a similar form factor to my weller wxmp

image

With the temperature set at 300 degC it struggled a little to melt leaded solder on a copper clad board.

 

When I adjusted the temp to 330 degC the same temp I use on my weller wxmp, Id say its thermal performance felt similar (no scientific evidence).

 

The only obvious criticism I have thus far is the included silicone USB cable is a little on the short side. If the cable was 30 cm longer, I think it would be long enough. I am hopping to find a powerbank that will power this iron, at which point the USB cable length would not be an issue.

 

It also didn’t include a travel or storage pouch…

 image

But that is also okay, I think I am going to try and put together an electronics first aid kit (I have the soldering iron covered).

  • Sign in to reply
  • Cancel
Parents
  • cstanton
    cstanton over 3 years ago

    If I ever get to go to DEF CON I think I'll have to take one of these with me for some badge life hacking. I wonder if airport security will care much for it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton over 3 years ago

    If I ever get to go to DEF CON I think I'll have to take one of these with me for some badge life hacking. I wonder if airport security will care much for it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • baldengineer
    baldengineer over 3 years ago in reply to cstanton

    Everyone that takes gear to DEF CON worries about their local airport security. There are almost no stories of anyone having to give up tools.

    I've traveled around the world with various electronics tools and have never had an issue. In fact, the ONLY thing I've ever traveled with that caused issues was a microphone. Nearly every security checkpoint would ask me to remove it. I asked a friendly agent why. He showed me the x-ray image. On the x-ray it looked like a hand grenade.

    That said, it's not hard to find a free station in the hardware village--even when it seems totally packed! But, I would still at least bring supplies.