Member's Forum What would you put in a solder aid or emergency maker kit?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 626 subscribers
  • Views 30948 views
  • Users 0 members are here
Related

What would you put in a solder aid or emergency maker kit?

scottiebabe
scottiebabe over 3 years ago

If you are away from your workbench either in your backyard or perhaps 100's km away and you need to repair or modify your project or prototype what would be the essential tools and components needed?

I am taking some inspiration from these low cost 100-in-1 solder tool kits:

image

Here is my Second Draft Attempt:

Tools Consumables Components Electronics Jellybeans Tin
Portable soldering iron Solder (Your choice leaded) USB Wall Wart spdt switch
Solder sucker Solder braid USB Power Bank banana jack
Multimeter Heat shrink USB A - micro cable banana plug
Ruler Hot glue stick USB C - C cable 1n4007 x4
Wire strippers (your-choice) Zip-ties 100 thou headers 1N4148
Side cutters Tape (your-choice) Dupont jumpers 2n3904/2n3906
Pliers Flux A piece of perf board Power N-FET
Tweezers Bismuth Solder A piece of copper clad board Axial Resistors 100,1k,10K,100K Qty 10 each
Telescoping Magnet  Flux A piece of 1.5 mm plywood Some leaded LEDs
Knife (not sure what kind)  Cyanoacrylate Glue Hookup wire (24AWG stranded likely) 7805
Bic lighter Heat Sink Sil-Pad 10 cm of cat-x network cable LM317 and potentiometer
Miniature screw driver set (the interchange bits)   small spool of 30AWG Kynar wire A few electrolytic capacitors
Alligator clip leads Copper Tape Tin of Electronics Jellybeans LM324 or LM358
Soldering Iron Stand Polydoh RPI Pico 0805 SMD Assortment
Tip Cleaner (your-choice) Blu-tac extension cord
Sharpie Stress-relieving candy power bar
Flash Light Electronics Cleaner 9V battery
Safety Glasses ESD Bag 4-40 machine screws
  Nail Polish
 
Plastic Prying 
Spudger
Scissors
Vise Grips
crescent wrench
Full Size Screw drivers
Helping Hands
Earth Ground Plug
ESD Mat
ESD Wrist Strap

I have pretty much all of these items in quantity already. So I can easily appropriate some of them to my emergency maker kit! Like wind the wires listed onto a small bobins, etc

baldengineer is also ahead of me with 0805 smd components suggestion! 

I'm trying to not go overboard with handtools but I think I could use some more...

Perhaps there are low cost modules you shouldn't leave home without? lol...

This is definitely a work in progress...

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 3 years ago

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    I don't hot glue enough for a glue gun to make it into the emergency kit, but I can see others justifying having it in their kit. Most of the time I heat up the end of a glue stick with hot air or a lighter than put a big gob to hold something down. When I hot glued a thermistor to a solar panel I used a magnifying glass to heat up the hot glue, no batteries required! 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to scottiebabe

    I recently used hot glue to fashion a strain relief (along with heatshrink) when connecting wire to a Kelvin clip - the wire needed to be immobilized to prevent stress on the solder joint:

    image

    Sometimes it is hard to beat the hot glue solution.

    How would you tackle this build?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to shabaz

    A quick solution might be to drill through the plastic clip handle from the outside and through the copper inside. Insert the stripped cable from the outside through the hole and solder to the copper on the inside. Fold the insulated cable against the outside of the clip handle then slip some glue-lined heat-shrink over the cable and clip handle and heat to secure it in place.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave

    I love glue-lined heat-shrink : ) It's a brilliant problem-solver. 3D printing would be a nice solution.

    Incidentally these sorts of Kelvin clips are really nice. I have slightly more expensive ones, but these ones are a better size, and have a good feel to them, just the right amount of springiness : ) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to shabaz

    Ah, now we get the full picture.. Looks like Doug's been busy with the cutting tools Slight smile

    I think you could 3D print a form that would nicely match the profile of the end of that handle and then transition it into a round cable exit sleeve (using a tapered extrude from a square profile to a round profile).

    You could then either lightly glue the mating faces of the 3D printed form onto the end of the clip handle or use glue-lined heatshrink (or both for 'belt and braces') then use smaller diameter heatshrink onto the exiting cable to hold it and form a strain relief onto the test lead.   

    You could go one step further and 3D print a form for inside the clip handle and have a hollow spigot pass through the U-shaped opening to connect the internal and external 3D printed parts together, sandwiching the clip handle between in the process.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 3 years ago in reply to shabaz

    Ah, now we get the full picture.. Looks like Doug's been busy with the cutting tools Slight smile

    I think you could 3D print a form that would nicely match the profile of the end of that handle and then transition it into a round cable exit sleeve (using a tapered extrude from a square profile to a round profile).

    You could then either lightly glue the mating faces of the 3D printed form onto the end of the clip handle or use glue-lined heatshrink (or both for 'belt and braces') then use smaller diameter heatshrink onto the exiting cable to hold it and form a strain relief onto the test lead.   

    You could go one step further and 3D print a form for inside the clip handle and have a hollow spigot pass through the U-shaped opening to connect the internal and external 3D printed parts together, sandwiching the clip handle between in the process.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • beacon_dave
    beacon_dave over 3 years ago in reply to shabaz

    A quick solution might be to drill through the plastic clip handle from the outside and through the copper inside. Insert the stripped cable from the outside through the hole and solder to the copper on the inside. Fold the insulated cable against the outside of the clip handle then slip some glue-lined heat-shrink over the cable and clip handle and heat to secure it in place.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave

    I love glue-lined heat-shrink : ) It's a brilliant problem-solver. 3D printing would be a nice solution.

    Incidentally these sorts of Kelvin clips are really nice. I have slightly more expensive ones, but these ones are a better size, and have a good feel to them, just the right amount of springiness : )