Products
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
Member's Forum Wat is the oldest chip in your parts bin?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 627 subscribers
  • Views 6339 views
  • Users 0 members are here
  • MC6800
  • 2708
  • z80
  • old ICs
  • old chips
Related

Wat is the oldest chip in your parts bin?

dougw
dougw over 3 years ago

I came across some old and famous chips in one of my parts cabinets. Does anybody else keep old chips? and why?

Note that these were pretty expensive when they were purchased, especially the gold plated ceramic chips.

I expect most of these are part numbers that everyone has heard of.

Have you designed with any of these famous chips?

Brownie points if you can figure out the date codes.

image

image

What chips are buried in your archives?

  • Sign in to reply
  • Cancel
Parents
  • jc2048
    jc2048 over 3 years ago

    Here's one of a similar vintage. The carbon-loaded anti-static foam is now crumbling.

    Was that the UART peripheral in their set of chips?

    image

    This next one is a very curious beast. I think the 1771 was a disc controller, but why was there a painted-over window on the top? Even stranger, there's one underneath, too. Perhaps they were programming their own chips.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 3 years ago in reply to jc2048

    This is the Nat Semi version of the 1771 on a board. That date code would be week 45 of 1979 (I was doing this in the early 1980s). There's a hugh cavity there, so maybe that's two chips side by side. It would explain why the Western Digital part has windows top and bottom if their part had two die back to back.

    image

    The 1771 had an internal data separator that didn't work very well, so this was the mod to get it going.

    image

    I had that working with a 6502 as the processor, a single-sided 8" disc drive, and fig-FORTH.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 3 years ago in reply to jc2048

    This is the Nat Semi version of the 1771 on a board. That date code would be week 45 of 1979 (I was doing this in the early 1980s). There's a hugh cavity there, so maybe that's two chips side by side. It would explain why the Western Digital part has windows top and bottom if their part had two die back to back.

    image

    The 1771 had an internal data separator that didn't work very well, so this was the mod to get it going.

    image

    I had that working with a 6502 as the processor, a single-sided 8" disc drive, and fig-FORTH.

    • Cancel
    • Vote Up +4 Vote Down