Member's Forum Wat is the oldest chip in your parts bin?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 592 subscribers
  • Views 5434 views
  • Users 0 members are here
  • MC6800
  • 2708
  • z80
  • old ICs
  • old chips
Related

Wat is the oldest chip in your parts bin?

dougw
dougw over 2 years ago

I came across some old and famous chips in one of my parts cabinets. Does anybody else keep old chips? and why?

Note that these were pretty expensive when they were purchased, especially the gold plated ceramic chips.

I expect most of these are part numbers that everyone has heard of.

Have you designed with any of these famous chips?

Brownie points if you can figure out the date codes.

image

image

What chips are buried in your archives?

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy over 2 years ago +8
    I used to design with a lot of Signetics parts in the 70's. I've got one of the early 555 parts. Shown here with a 566 VCO and 5556 opamp. I probably have some of the 56x series PLLs around somewhere…
  • baldengineer
    baldengineer over 2 years ago +6
    I was excited because I thought I'd have a real contender. But, today is the first time I ever looked the date code, which is on the bottom. It's from a run in 1980. So I probably have MOS 6502 chips…
  • Jan Cumps
    Jan Cumps over 2 years ago +6
    oldest I had: image source . I don't have that kit anymore.
  • misaz
    misaz over 2 years ago in reply to scottiebabe

    In my case it is the same. My most probably oldest chip is UCY7406 containing 6 invertors.

    image

    This chip we used at high school for basic logic labs, but in personal project I never used it. The oldest chip which I bought and used for leaning in my beginings is ATmega16.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 2 years ago

    I have several old chips in my collection, which makes a lot of sense as I started my electronics hobby/career in the early 70's.  I have several high-power vacuum tubes (from commercial FM transmitters, some up to 5000 Watts).  In IC's I have several gold cased ICs, including simple logic gates and such from, my early years in the military electronics field and many early processors and other long ago obsolete components.  I have a bunch of old germanium and silicon chips from some early work I did in electronic music and synthesizers.  I will have to see if I can dig up a specimen to share pictures. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to scottiebabe

    I wish I had an LM109/LM309 more closely related to https://en.wikipedia.org/wiki/Bob_Widlar 

    image

    Random TLL inverter

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 2 years ago

    Here's one of a similar vintage. The carbon-loaded anti-static foam is now crumbling.

    Was that the UART peripheral in their set of chips?

    image

    This next one is a very curious beast. I think the 1771 was a disc controller, but why was there a painted-over window on the top? Even stranger, there's one underneath, too. Perhaps they were programming their own chips.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 2 years ago in reply to beacon_dave

    That is an amazing amount of effort especially writing your own dissambler.  The programmers of yesterday did seem to like jumping in and out of subroutines.  I formed that opinion, anyway, after seeing the dissasmbly of some Intellivision games.  And truth be told I couldn't extract enough meaning from the generated code to make any sense of it.  Best of luck if you ever resume this project again.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    I have a lot of IC's from the early 1970's.

    Many have gold coatings, so I hold on to them because they are probably quite valuable by now.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago in reply to scottiebabe

    I will search my stash, we might get lucky.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to dang74

    Actually, I found that was one of the easier parts as Hitachi had a datasheet on the HD6303 so I had the opcode map and the number of operands each opcode expected. I knew where the processor looked for the interrupt vector table in memory so the value stored there at told me the address where the executable code started. From there it is just a case of looking up the opcode and then finding how many operands it expects and away you go. It was a bit tedious as the data sheet was scanned so no quick cut and paste into the program. Add in a few extra routines to calculate addressing offsets to make it more readable. In-line data can be an issue. Also keeping an eye on the interrupt vector table can identify start addresses of other code blocks.  

    If you want effort, then that was months of looking at data captures from a scope trying to figure out patterns in the data. It turned out that the comms was asymmetrically encoded so the few ASCII characters in the config section were initially obfuscated. Then finally once I had identified the encoding method there was a 'Twin Peaks moment' 

    https://www.youtube.com/watch?v=mbi7rq-TSk8&t=78s

    as the hex sequence for the Program ID and data ID strings finally matched one of the data captures and confirmed I was really on the right track.

    If the code was originally generated from an optimising compiler, then it often can often be hard to follow as the optimisation can save program cycles by doing certain procedures in rather non-intuitive ways. Also by having lots of near jumps you can reduce the overall code size to fit in the limited memory by reusing code blocks, however once again it makes it a lot harder to follow.

    It would make life easier I think if I had a way of turning the listing into a graphical diagram with the blocks of code linked by the jumps such that you could slide things around so that the related sections were next to each other. Also a way of labelling and commenting what you had identified so far. I think that's what the call 'data graph' structures in programming lingo ?  I once saw this done manually with string and post-it notes !

    If I was a bit further along the line, then I might have given the LabVIEW challenge a go using it to connect to the ECU (or rather the ECU protocol simulator that I have also written as part of this project). However  I'm not sure what is involved in getting LabVIEW to talk to the ECU protocol and parse the data.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to jc2048

    Yes - the ACIA. I also have a bunch of chips in crumbling black anti static foam like what your chip is on.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 2 years ago

    I used to design with a lot of Signetics parts in the 70's.  I've got one of the early 555 parts.  Shown here with a 566 VCO and 5556 opamp.

    image

    I probably have some of the 56x series PLLs around somewhere.  The 566 is the VCO from one of those parts.

    The earliest part that was easy to find was a 7400 series part from TI.

    image

    And, of course I used a lot of opamps.  Here are a couple of National Semi parts (never used spares) - an uncompensated 709 and a dual 747.

    image

    I'm sure I have lots of other old stuff somewhere.  Back in those days I used a lot of MECL from Motorola and analog parts from Fairchild and TI.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
<>