Member's Forum Seeking Your Feedback on a Beat Our Board Design Challenge - Grand Prize $5,000
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 625 subscribers
  • Views 4605 views
  • Users 0 members are here
  • design challenge survey
Related

Seeking Your Feedback on a Beat Our Board Design Challenge - Grand Prize $5,000

rscasny
rscasny over 3 years ago

I've been in discussions with a component supplier who would like to sponsor a Design Challenge.

But its vision of the Design Challenge is a little different than how element14 typically administers a Design Challenge. I want to tell you the details below. I would really appreciate you voting in the polls and offering feedback on the challenge. Thanks.

Randall
-element14 Community Team


What is the Beat Our Board Design Challenge?

The goal of PI Beat Our Board Design Challenge is for the participants to design a board that improves or beats the sponsor's DER-953 board. Below, I've posted a short video and a schematic of this RDK, as well as the datasheet.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

image

How Applicants are Selected as one of the Top 10

The Top 10 submissions get to advance to the next stage and will be given the DER-953Q plus a $250 shopping cart to buy materials – fulfilled by Farnell. The sponsor or its representatives will judge the finalists. They are awarding $5,000 to the grand prize winner and $2,500 to the 2nd place winner.

The enrollment period will last 6 weeks.

What they need to show to be one of the top 10

To be selected as one of the Top 10, the applicant needs to show the following:
• Topology / switch type
• Transformer size
• Preliminary schematic

The length of the challenge is about 6 months (ends June 2024).

Here are the criteria to win:

• Cannot use InnoSwitch
• Beat the efficiency – 10%, 25%, 50% and 100% no-load
• 40-500 V DC input
• Size/ volume of board must be same size or smaller
• Must meet thermals – 85 degrees Celsius – no heatsink
• No optocouplers
• Component count
• No-load consumption
• Automotive qualified components only
• Transformer exempt
• Up to and no more than a 6-layer PCB
• Specify PCB stack up weight per sq foot- 2oz 1oz 1oz 1oz 2: Maximum copper thickness on top and bottom layers
• Overload power current limit = 8.1 A

What do you think of this challenge? I invite you to offer your thoughts in the comments section below.

I also invite you to vote in the following polls:



  • Sign in to reply
  • Cancel
  • michaelkellett
    michaelkellett over 3 years ago

    There is a trick or typo in the target spec - PI's board accepts 150 - 500V DC but the challenge is for 40-500V DC.

    But on to the substance.

    If I were to accept this task as a commercial project (which I probably wouldn't as it stands because it's definitely and Automotive spec project and I haven't worked in that domain for  along time).

    But if I were to take it on I would be looking at charging of the order of £25k for the work - might be double - that was a 5 minute quote with an asymmetric 200% tolerance !

    So it looks a bit like an engineering equivalent of those dance marathons that desperate people entered in the 1930s because they needed the prize money.

    en.wikipedia.org/.../Dance_marathon

    Misaz summed it up in 7 words:

    misaz said:
    It is very cool but too hard

    BTW, you need some pretty good and fancy test gear to develop this - like the 900V power supply.

    I think the basic idea of a challenge is OK - but this one is much too hard for a fun event.

    A much better challenge might be to do something useful with  a handful of PI's Innoswitch chips.

    MK

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • strb
    strb over 3 years ago

    As others already stated,I also think that could be better decreasing the overall kits number while increasing design/development support for challengers (for example increased initial budget or sponsored PCBs).
    This design challenge is very cool but also quite hard. I like challenges (and this one is definitely outside my confort zone) but this one I think it will be too hard for me to carry out in a proper way. Also, the test equipment needed to evaluate such design is no joke. Time availability could also play a big role here (and for me it will since I've already scheduled other important things for next year).

    I voted for:
    - "After reading the information provided above, are you interested in joining this challenge?" : Maybe. I'm interested? Yes, I like this challenge. Will I apply? Probably not. (but good luck to all future challengers!)
    -"Are you working as an Automotive Power Design Engineer?" No. I have little experience with some switching converters and motor power stage but I would not call myself a power electronic engineer
    -"On your design workbench, do you have access to at least 40VDC": Yes, my power supply can go up to about 60V if I remember correctly. Still, I don't think that's enough to evaluate this specific design request. A lot of other equipment will be needed too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Here's another idea, just to brainstorm a bit;

    It could be attractive to customers to see the actual use of the PI product, for instance, what it is like designing for that unusual IC package, and what real-world transformer (or custom one) works, and what is practical in terms of PCB size and PCB technologies, and what measurements were taken. This would (I hope) be interesting to the manufacturer too; they could learn a lot since nobody will know their product better than customers who get their hands dirty with it.

    Trying to compete with other manufacturer parts is for sure a valid challenge, but it's a type of challenge that might help in initial device selection but won't help customers in using the PI product.

    Since it's a lot of work, and 10 contestants who will do it justice with the custom work (PCBs, etc that will be required) will be hard to find, perhaps a method without a contest could be better, that way only one person (or say two persons) need to be found, and let them have lots of latitude in what they design, and providing they do produce the material, then for them to be awarded the full amount (it would easily consume a couple of months of work, so instead of June 2024, material could be available sooner this way, and if customers benefit from it, then PI could run a second campaign of some sort - so it's quite efficient. It would cost the same - might as well let both people (if there are two) be awarded the identical full amount if they produce the content; let them not feel they are competing against each other so that they can share material as they work.

    If it were me (I am not saying I would apply, but I might be tempted if I could concentrate on the things that I feel would interest me and customers, rather than try to meet a specification that doesn't meet my needs) I'd be interested in making a reliable power supply (perhaps several of the PI devices, OR'ing them together) with the benefit of higher output current at lower input voltages.

    It might not be what all their customers might want (but I bet manufacturers only know what a subset of customers do with their products; and if PI really wanted precise alignment then they might benefit from looking for a case study with the customers that they might already be working with). So, in this case, perhaps it is not a negative thing that it will be hard to find 100% alignment; if the application is still likely to reveal relevant stuff - for instance, I would say that's quite realistic from a heat generation point of view, having more heat sources on a board than just a single power supply.

    Others might be interested in (say) using the chip for a different output voltage, perhaps, and maybe that might reveal valuable information to customers, about how versatile that chip is (or not). 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago

    Sorry, the workscope is not in my talent quiver and too much like real work. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 3 years ago

    It is very cool but too hard, I think. Maybe it is hard just to me, but I think it is very hard in comparison with standard design challenge, when you can take just a Arduino and do something. I consider it very hard also because DER-953Q design is realy nice. Power Integrations spend lot of time with designing it and datasheet shows all evaluation results. I think there is very low chance that someone make something better.

    I do not understand the point "Cannot use InnoSwitch". At begining you wrote that we can win by improving their design, but later it seems that we should create (new) design using competittor products practicaly showing that it is impossible to make better design. That is interesting.

    You can also consider sending member result (final board) to Power Integration for propper (and equal/fair) evaluation under same terms (high voltage tests, tests at thermal limits, ...). In other words sponsoring shipping from member to Element14 (or Power Integration), basicaly the reverse way you send packages to us.

    I think 10 sponsored kits are too much. Because of complexity I gues that no more than 5 kits are necessary. Instead you can consider sponsoring PCB manufacturing.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
<