Member's Forum Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 623 subscribers
  • Views 7170 views
  • Users 0 members are here
  • wind
  • hydrogen
  • question of the month
  • green technology
  • efficiency
  • solar
  • renewable energy
Related

Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?

dychen
dychen over 2 years ago

e14 Question of the Month

Consumers are making the move to renewable energy, however, there is still a lot of dependence on fossil fuels.  Take the poll and in the Comments section, let us know what you think can be done to make the shift to renewable energy easier.

  • Sign in to reply
  • Cancel
Parents
  • BigG
    BigG over 2 years ago

    source of image: amazon

    As we start to see more and more of these type of USB power sockets around the place, maybe the question is... why are these sockets only 5V DC. Could we get more use-cases for 12V and maybe 24V for homes and offices, especially if every building had a renewable energy source and a big old battery. One feeds of the other, so to speak. Then I suppose, the other question, if this renewable energy source plus battery is working well then I wonder... would we still need AC power sockets in every room in the home or in the business.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 2 years ago

    source of image: amazon

    As we start to see more and more of these type of USB power sockets around the place, maybe the question is... why are these sockets only 5V DC. Could we get more use-cases for 12V and maybe 24V for homes and offices, especially if every building had a renewable energy source and a big old battery. One feeds of the other, so to speak. Then I suppose, the other question, if this renewable energy source plus battery is working well then I wonder... would we still need AC power sockets in every room in the home or in the business.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • bradfordmiller
    bradfordmiller over 2 years ago in reply to BigG

    Many years ago, pop 'tronics ran an article on smart plugs that eliminated the need for power supplies in appliances. Even washing machines could use DC moters because they'd just request alternating current synchronized with reversing their drums. Basically you'd get a couple hots and a digital line to request a voltage and amperage from a smart panel at your distribution point.

    I suspect this never went anywhere because the initial cost was high, and appliance makers didn't want to commit to it until it was already ubiquitous. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to BigG

    cost of the cabling - lower voltage means higher currents -> higher diameter conductors are needed to keep the same voltage drop (percentage) across the installation. There is the saying that  there are DC powered server rooms somewhere (and maybe telecom switches were powered from 48V) but this involves very high diameter power lines to keep voltage drops in acceptable levels. It is the same as in PoE (power over ethernet) when voltage is (IIRC) 48V to keep energy waste in line.