Member's Forum Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 588 subscribers
  • Views 6446 views
  • Users 0 members are here
  • wind
  • hydrogen
  • question of the month
  • green technology
  • efficiency
  • solar
  • renewable energy
Related

Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?

dychen
dychen over 2 years ago

e14 Question of the Month

Consumers are making the move to renewable energy, however, there is still a lot of dependence on fossil fuels.  Take the poll and in the Comments section, let us know what you think can be done to make the shift to renewable energy easier.

  • Sign in to reply
  • Cancel

Top Replies

  • balajivan1995
    balajivan1995 over 2 years ago +3
    I like this question and the order the choices are presented, these are all the things that comes to my mind when it comes to adapting renewable energy sources. The main problem is ROI made on the purchase…
  • michaelkellett
    michaelkellett over 2 years ago +3
    It's all these things and more. We've got over 100 years of investment in the existing infrastructure - it's a huge task to change it all and it just can't happen overnight. There hasn't been anything…
  • Andrew J
    Andrew J over 2 years ago +3
    Click-bait articles from know-nothing, investigating-nothing people. Mainstream media articles with poor and lazy journalism doing the same thing. Lack of willingness to find out things for oneself. Regurgitating…
Parents
  • robogary
    robogary over 2 years ago

    From real calculations, solar at my home does not provide ROI. There is a mountain behind the house westbound. We only get direct sun for half a day. The local power company uses hydro as part of the energy mix and my electricity prices are relatively low , altho increasing what feels exponentially. 

    What I find ironic and hilarious is the Special Interest Groups, media, bureaucrats, are screaming for Green Energy ---- then when a Wind Turbine Project or Solar Project site is selected, other Special Interest Groups, media, bureaucrats, start screaming - NOT HERE ! NOT HERE ! its disrupting the three toed paisley nano-salamanders mating drive, its making the whales nervous, its destroying the view of the natural forest and mountains, the project devalues my Martha Vineyards spring vacation home and the winter vacation home in Florida,  those power generators are ugly, blah blah blah   

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller over 2 years ago in reply to robogary

    I think a case can also be made that any solution that requires subsidies implies it is not an economically feasible solution. When "renewable energy" makes sense, it will be less expensive than "non-renewable" sources (including, e.g., the time to recharge one's vehicle for one data point), and people will naturally prefer it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to bradfordmiller
    This reply was deleted.
    • Cancel
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to bradfordmiller

    I suppose that a case like that could be made.  A case could just as easily be made that subsidising allows for earlier investment to build the infrastructure and roll it out.  Renewable energy does make sense but isn't yet capable of providing enough of (all? most?) countries needs yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago in reply to bradfordmiller

    In fact - another thing that burns my britches, I have sensor controlled outdoor light fixtures that require incandescent bulbs. LED bulbs wont work in them. Government outlawed incandescent bulbs but sellers are still selling their incandescent lamp inventory. I've replaced the cheap fixtures, but the big brass porch lights are getting by on whats left of any incandescent laying around the house.  One has a powder room bulb in it.   :-) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller over 2 years ago in reply to anniel747

    Behavioral economics is the science of why people make certain choices; not all branches of economics presume rationality :-)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • electronicbiker
    electronicbiker over 2 years ago in reply to robogary

    Glad to hear incandescent bulbs are still available! Without them, how am I supposed to check the speed of my record deck?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • electronicbiker
    electronicbiker over 2 years ago in reply to robogary

    I have several LED bulbs that run hot, so much so that I have to wait for them to cool down before extracting them. I guess this is because of the 230V available, 225V of it has to be dumped somewhere to prevent destruction of the LEDs. I've ignored RMS etc to keep this short, I'm running late as it is...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago in reply to electronicbiker

    They don't really work like that. Mains powered bulbs containing a small number of LEDs use some kind of switching regulator to convert rectified mains to a suitable voltage to power the LEDs. These regulators are often not very reliable (being built from very cheap parts) but are reasonable efficient.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • electronicbiker
    electronicbiker over 2 years ago in reply to michaelkellett

    Hi michaelkellett, thanks for the reply. I know that most use switching regulators these days, and some LED bulbs run at quite low temperatures. But others do not, and I wonder where all the excessive heat comes from. Something, somewhere, is being over-driven. Maybe the thyristors or triacs are not being switched fast enough.

    I also have some where the incoming AC is split so that a chain of LEDs light up during one half-cycle and the other chain on the other half-cycle. When they go a bit dim, it usually means that one of the chains has overheated just a little bit too much.

    LED room-lighting is not popular with photographers. Digital cameras can get quite upset by the spikey nature of switch-mode light.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to electronicbiker
    electronicbiker said:
    Glad to hear incandescent bulbs are still available! Without them, how am I supposed to check the speed of my record deck?

     DIY LED Stroboscope to Check Turntable Speed 

    What a time to be alive Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to electronicbiker
    electronicbiker said:
    Glad to hear incandescent bulbs are still available! Without them, how am I supposed to check the speed of my record deck?

     DIY LED Stroboscope to Check Turntable Speed 

    What a time to be alive Slight smile