Member's Forum Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 549 subscribers
  • Views 5781 views
  • Users 0 members are here
  • wind
  • hydrogen
  • question of the month
  • green technology
  • efficiency
  • solar
  • renewable energy
Related

Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?

dychen
dychen over 2 years ago

e14 Question of the Month

Consumers are making the move to renewable energy, however, there is still a lot of dependence on fossil fuels.  Take the poll and in the Comments section, let us know what you think can be done to make the shift to renewable energy easier.

  • Sign in to reply
  • Cancel

Top Replies

  • balajivan1995
    balajivan1995 over 2 years ago +3
    I like this question and the order the choices are presented, these are all the things that comes to my mind when it comes to adapting renewable energy sources. The main problem is ROI made on the purchase…
  • michaelkellett
    michaelkellett over 2 years ago +3
    It's all these things and more. We've got over 100 years of investment in the existing infrastructure - it's a huge task to change it all and it just can't happen overnight. There hasn't been anything…
  • Andrew J
    Andrew J over 2 years ago +3
    Click-bait articles from know-nothing, investigating-nothing people. Mainstream media articles with poor and lazy journalism doing the same thing. Lack of willingness to find out things for oneself. Regurgitating…
  • shabaz
    shabaz over 2 years ago

    Probably another issue is that no matter how efficient and lower-cost renewable energy becomes, if energy usage always rises, then it's hard for the technology improvements and supplies to keep up, meaning that traditional energy sources continue to be needed, too.
    The UK has an intriguing solution to this: let manufacturing decline. It might destroy jobs and push costs up, but it will reduce energy usage to an extent! : )

    Also, governments' easiest tools to make people introduce changes to reduce energy waste or to use other energy sources is sadly allowing prices to rise massively. Of all electricity generation, a tiny figure is useful. The rest is wasted in creating and distributing it. But, even if continual improvements are made, it will only delay the point at which more capability is required. So consumption (and waste at the consumption end, whether industrial or residential or otherwise) is super important, too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • redcharly
    redcharly over 2 years ago in reply to robogary

    The same happens in Italy, It's quite impossible to install  solar panels or wind turbines  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz
    shabaz said:
    "lack of political will"

    I like to translate that into "lack of everyone's will" in most countries.

    We all have political parties that want to move faster. We don't vote them into power. (Because we know it 'll hurt?)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to BigG

    Overall I think PoE saves energy, because it provides the granular visibility and control, super-easy to switch off power when it's not required!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    From my analysis of the situation, renewable energy has a place within the energy space, but is not yet ready to supplant traditional sources of energy.

    The debacle in Texas a couple of years ago aptly exposed the current weakness of the renewable capability.

    People died because the Texas grid did not have emergency power generation capability and the glaring fact that Texas did not have a compatible grid with any of their neighbors.

    These glaring errors were very predictable given their lack of risk analysis and adequate backup capability.

    You have to understand that it takes time to mature a new technology so that it can supply reliable energy.

    I have faith that renewable energy will eventually get to a level of maturity where it can indeed supplant the fossil fuel sources, but we are talking decades, not a few years.

    A lot of people are pushing this technology into production, and it is just not ready to deliver on its promises.

    Please lower your expectations, there are no immediate miracles.

    Everybody just stop, take a deep breath, and then use some common sense.

    It was decades before coal generated power was reliable enough to build out a power grid and it took decades before everyone who wanted power had access.

    Fifty years ago, I knew a local family who had still not connected to the power grid, even though it had been available to them for decades.

    So stop trying to put this horse into the race too quickly.

    We will get there eventually, patience is required.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Magurch
    Magurch over 2 years ago

    The #1 problem is our power grid can't handle the load and would cost trillions to update so it could.. it's almost impossible and would take decades.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Magurch

    decades would be nice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago in reply to Christopher678

    Not necessarily.

    People are blaming fossil fuels for an issue that they are not guilty.

    Humans are predictable animals, they continue to use what is cheapest until it becomes too expensive.

    Renewable energy is significantly more expensive than currently used fossil fuels.

    Most systems that use fossil fuels can change to use hydrogen, which is relatively easy to obtain.

    All of the infrastructure for fossil fuels is adaptable for hydrogen use.

    Therefore, the logical and most cost effective way forward is to begin integrating hydrogen as a fuel in combination with renewable energy sources.

    That solution enables the world to take advantage of existing investments and keep energy costs to a reasonable level while maintaining reliable energy.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago in reply to shabaz

    Politicians follow votes and money.

    They pander to the renewable crowd to get easy votes.

    The deal with the energy companies because they have money.

    When the system breaks like it did in Texas, they always find someone else to blame.

    Face it, if you had their job, you would do the same.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago in reply to Magurch

    The grid is being gradually updated every year.

    As you point out, the time to replace everything that needs fixed is long as the cost is high.

    Change requires patience and money.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>