Member's Forum Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 556 subscribers
  • Views 5907 views
  • Users 0 members are here
  • wind
  • hydrogen
  • question of the month
  • green technology
  • efficiency
  • solar
  • renewable energy
Related

Question of the Month: Which of the following do you think is the biggest barrier to moving to use more renewable energy sources?

dychen
dychen over 2 years ago

e14 Question of the Month

Consumers are making the move to renewable energy, however, there is still a lot of dependence on fossil fuels.  Take the poll and in the Comments section, let us know what you think can be done to make the shift to renewable energy easier.

  • Sign in to reply
  • Cancel

Top Replies

  • balajivan1995
    balajivan1995 over 2 years ago +3
    I like this question and the order the choices are presented, these are all the things that comes to my mind when it comes to adapting renewable energy sources. The main problem is ROI made on the purchase…
  • michaelkellett
    michaelkellett over 2 years ago +3
    It's all these things and more. We've got over 100 years of investment in the existing infrastructure - it's a huge task to change it all and it just can't happen overnight. There hasn't been anything…
  • Andrew J
    Andrew J over 2 years ago +3
    Click-bait articles from know-nothing, investigating-nothing people. Mainstream media articles with poor and lazy journalism doing the same thing. Lack of willingness to find out things for oneself. Regurgitating…
Parents
  • BigG
    BigG over 2 years ago

    source of image: amazon

    As we start to see more and more of these type of USB power sockets around the place, maybe the question is... why are these sockets only 5V DC. Could we get more use-cases for 12V and maybe 24V for homes and offices, especially if every building had a renewable energy source and a big old battery. One feeds of the other, so to speak. Then I suppose, the other question, if this renewable energy source plus battery is working well then I wonder... would we still need AC power sockets in every room in the home or in the business.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to BigG

    cost of the cabling - lower voltage means higher currents -> higher diameter conductors are needed to keep the same voltage drop (percentage) across the installation. There is the saying that  there are DC powered server rooms somewhere (and maybe telecom switches were powered from 48V) but this involves very high diameter power lines to keep voltage drops in acceptable levels. It is the same as in PoE (power over ethernet) when voltage is (IIRC) 48V to keep energy waste in line.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 2 years ago in reply to JWx

    Yes, scalability would be an issue in some larger buildings like apartment blocks. For homes though, I like the idea of having a 48V PoE as a backbone. It may not be perfect but it could be a workable solution. This will make setting up connected (smart home) devices so much easier for the not-so-smart end user.

    Maybe Single Pair Ethernet (SPE) with POE (not sure if this is actually viable) could also lower cost of cabling.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to BigG

    Overall I think PoE saves energy, because it provides the granular visibility and control, super-easy to switch off power when it's not required!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago in reply to BigG

    Overall I think PoE saves energy, because it provides the granular visibility and control, super-easy to switch off power when it's not required!