Products
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
Member's Forum USB Memory stick and freezing temperatures
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 628 subscribers
  • Views 3462 views
  • Users 0 members are here
Related

USB Memory stick and freezing temperatures

Workshopshed
Workshopshed over 2 years ago

My car has an in built sat nav and to update it there is a process that involves copying some very large files onto a USB stick and sticking that in the slot in the car. The car needs to be running whilst updating.

I've a long trip (for which I don't need maps) coming up so I left the memory stick in the car overnight so I don't forget it.

But

The temperatures here are dropping to -4°C over night.

So my question is. Will this cause me any problems for the memory stick? Don't intend on repeating this regularly so it is a one off.

  • Sign in to reply
  • Cancel
Parents
  • misaz
    0 misaz over 2 years ago

    Most probably it will work well. All flash chips which I have seen as far has working range set to standard -40 to 85°C. Possible very high humidity was the worse enviromental factor, I think.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • misaz
    0 misaz over 2 years ago in reply to misaz

    I checked some and it seems that vendors mention reduced temperature ranges on final products. For example, this (https://www.westerndigital.com/en-us/products/usb-flash-drives/sandisk-cruzer-blade-usb-2-0?sku=SDCZ50-032G-B35) has 0 to 45°C, but -4°C is still not very far from 0.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • misaz
    0 misaz over 2 years ago in reply to misaz

    I checked some and it seems that vendors mention reduced temperature ranges on final products. For example, this (https://www.westerndigital.com/en-us/products/usb-flash-drives/sandisk-cruzer-blade-usb-2-0?sku=SDCZ50-032G-B35) has 0 to 45°C, but -4°C is still not very far from 0.