Member's Forum What's inside a 20+ year old dimmer switch?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 623 subscribers
  • Views 6584 views
  • Users 0 members are here
Related

What's inside a 20+ year old dimmer switch?

scottiebabe
scottiebabe over 2 years ago

Not much. The dimmer function failed and only the switch function remained functional.

image

image

image

image

The schematic is the same as drawn by this author:

image

The Quadrac (an internally triggered triac, a triac + diac) failed short between all three terminals.

Searching for an X25783 datasheet led me to this,

image

https://images.100y.com.tw/pdf_file/31-Teccor-Quadrac.pdf 

A more common brand that may be similar could be the 

image

https://www.littelfuse.com/media?resourcetype=datasheets&itemid=b4817091-0710-4ac7-a446-a7ffcca0a634&filename=littelfuse_thyristor_q6008lth1led_datasheet.pdf 

The potentiometer used as a rheostat has a switch stacked on top.

Not much inside...

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    scottiebabe over 2 years ago

    Update! There was a party inside.

    The pot terminals flashed over to the case at some point...

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to scottiebabe
    This reply was deleted.
    • Cancel
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to anniel747

    Not sure when it happened or how. There appears to be about a 1.5 mm air gap between the tabs and case.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller over 2 years ago in reply to electronicbiker

    It's my understanding that 20+ year old electronics would have lead/tin solder, which generally would not form tin whiskers (unlike lead-free solder). REALLY old solder (think 1920s) did have whiskers, either because there wasn't enough lead or too much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • electronicbiker
    electronicbiker over 2 years ago in reply to scottiebabe

    Hi scottiebabe, sorry about the misunderstanding - I thought you were Scottish and lived in Scotland!

    So, ok, the 1.5mm gap should be fine at 110v. But I've just thought of something else...  Over a long period of time, soldered connections (especially when close together on a PCB) can exhibit a strange phenomenon caused by 'creepage'. This is where a soldered connection through holes in a PCB (amongst other places) will produce radial hair-like dendrites growing in length across the surface of the PCB. If they meet dendrites from another soldered connection then there may be trouble! I have seen solder connections where dendrites have grown all around them, looking like multipointed stars with very sharp points. The sharp edges around the ends of the through-pins used for connecting the two sides of a double-sided PCB are quite good at dendrite-growing, and an electromagnetic field helps to 'steer' them. Such as the ones produced by inductors.

    This is not a very common failure mode, but it can happen. If anything much more than a small current passes along a dendrite it immediately blows just like a fuse, thus destroying the evidence. One place where they might have formed is between two of the rivets holding the terminals in contact with the track on the pot.

    A lot depends on the age of components and PCB material. Conformal coatings on PCB's will usually prevent creepage effects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • electronicbiker
    electronicbiker over 2 years ago in reply to scottiebabe

    Hi scottiebabe, sorry about the misunderstanding - I thought you were Scottish and lived in Scotland!

    So, ok, the 1.5mm gap should be fine at 110v. But I've just thought of something else...  Over a long period of time, soldered connections (especially when close together on a PCB) can exhibit a strange phenomenon caused by 'creepage'. This is where a soldered connection through holes in a PCB (amongst other places) will produce radial hair-like dendrites growing in length across the surface of the PCB. If they meet dendrites from another soldered connection then there may be trouble! I have seen solder connections where dendrites have grown all around them, looking like multipointed stars with very sharp points. The sharp edges around the ends of the through-pins used for connecting the two sides of a double-sided PCB are quite good at dendrite-growing, and an electromagnetic field helps to 'steer' them. Such as the ones produced by inductors.

    This is not a very common failure mode, but it can happen. If anything much more than a small current passes along a dendrite it immediately blows just like a fuse, thus destroying the evidence. One place where they might have formed is between two of the rivets holding the terminals in contact with the track on the pot.

    A lot depends on the age of components and PCB material. Conformal coatings on PCB's will usually prevent creepage effects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • bradfordmiller
    bradfordmiller over 2 years ago in reply to electronicbiker

    It's my understanding that 20+ year old electronics would have lead/tin solder, which generally would not form tin whiskers (unlike lead-free solder). REALLY old solder (think 1920s) did have whiskers, either because there wasn't enough lead or too much.