Products
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
Member's Forum What was your first electronics project?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 50 replies
  • Subscribers 626 subscribers
  • Views 5988 views
  • Users 0 members are here
  • first electronics project
Related

What was your first electronics project?

dougw
dougw over 2 years ago

What was your very first electronics project?

Why did you take it on?

I think my first successful, non school-related electronics project was an electronic doorbell that would randomly play one of a whole (fixed) suite of sound effects and melodies or jingles.

After brief use as a doorbell, it eventually got used as toy, but "someone" couldn't stand the kids playing it non-stop, so it got tossed out....Disappointed

I built the project because I thought it was such a cool chip, (I still think it was cool) but it was many years ago and I can no longer recall the chip I used or find something that seems similar.

  • Sign in to reply
  • Cancel
Parents
  • dang74
    dang74 over 2 years ago

    I won't flatter myself to present this as a 'first project' but this bit of misadventure fits the general spirit of the topic.  To any of you younger readers, this tale harkens back to the pre-internet era before we had easy access to things like YouTube.  It's also a cautionary tale showing what happens when you combine an unquenchable sense of curiosity with a total lack of knowledge in the field your particular project falls into.

    Back when I was ten I had seen some experiments on TV where batteries were used to illuminate a light bulb.  I spent a good part of the day trying to replicate these results but the light bulbs I had access to could not be powered with the measly dry cell batteries I had salvaged from electronic toys.

    I knew I had to bring things up a notch.  Why fiddle around with batteries when there was a unlimited supply of electricity hiding in the walls.

    As a bit of foreshadowing I will have you know that a movie had come out around this time called Short Circuit.  So while the phrase had entered my ears I had no real concept of what a short circuit actually was.

    Back in the 80s my aunt was in the armed forces and was stationed in Germany.  For Christmas she had sent me a decorative lamp along with the adapter to convert its European plug to a North American one.  This adapter was going to be the key to unlock my experiment....

    I stripped a couple of garbage ties and jammed them into the adapter.  The other sides of the ties were secured to a trail of coins using clear Scotch tape.  The coins which were arranged on my carpet formed a trail leading to a light bulb.

    I wish I had the intuition then to have run the coins in two separate paths.  One path leading to the light bulb and one path returning from it.  But no, shortly after my garbage tie connections I had arranged the coins to converge into a single path.  You could say that 'the trap was set.'

    Around this time I had a sobering thought where the gravity of playing with AC power suddenly hit me.  Did I dismantle my setup and abandon the experiment?  No, instead I called on my little sister for moral support.

    We sat there a moment before I summoned the courage to plug the cord in.  The very moment the plug engaged we were startled with a frightening popping sound.  Worse still a little flame, not unlike that on a birthday candle, had formed on my carpet.

    Immediately I unplug the cord and begin to frantically blow out the flame.  Fortunately the little fire was extinguished before it could spread.  Miracuously enough there were no visible burn marks.

    "This could be a clean get away," I thought to myself.  That is of course if I had my sister's cooperation.

    Acting as the adult in the room, my seven year old sister finally says, "Okay, I won't tell mom and dad, but promise me you'll never do this again."

    Even in recent times I make the odd error but if I look back to these humble beginnings I realize I've come a long way.  We all have.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 2 years ago in reply to dang74

    On a similar note, when I was 4(?) I collected all sorts of objects to play with.  I had several of these key-like objects that were used to open coffee cans (removing a coil spring like ribbon of metal to separate the lid from the can).  I liked to play with these keys, imagining that they could unlock things like my cars and trucks.  One day I guess I decided to 'unlock' one of those little plastic rectangles on the wall (outlets).  I carefully inserted two 'keys' into the openings. A remember a flash of light, a violent muscle contraction and then bandaged little fingers.  How I didn't electrocute myself, I will never know.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 2 years ago in reply to dang74

    On a similar note, when I was 4(?) I collected all sorts of objects to play with.  I had several of these key-like objects that were used to open coffee cans (removing a coil spring like ribbon of metal to separate the lid from the can).  I liked to play with these keys, imagining that they could unlock things like my cars and trucks.  One day I guess I decided to 'unlock' one of those little plastic rectangles on the wall (outlets).  I carefully inserted two 'keys' into the openings. A remember a flash of light, a violent muscle contraction and then bandaged little fingers.  How I didn't electrocute myself, I will never know.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dang74
    dang74 over 2 years ago in reply to genebren

    Between you and Doug it appears that near electrocution has been a rite of passage for many of us.  So cute that you developed a fascination for these little coffee can keys.  Not related to electronics in anyway but as a kid I would get little umbrellas and plastic swords from my aunts and uncles.  There was a place in my home town that got creative in the presentation of their cocktails and food entrees.