Member's Forum Is electronic engineering dead?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 627 subscribers
  • Views 3599 views
  • Users 0 members are here
  • ic designers
  • integrated circuit designers
  • electronic engineering
  • fpga
  • student question
  • hardware design
Related

Is electronic engineering dead?

cstanton
cstanton over 2 years ago

I saw this question on Reddit, and I figured it was a good one to ask the element14 Community as a thought provoking query that may be on new engineering students minds:

"If we consider only circuit design for PCBs, almost all the complexity is moving toward integrated circuits (chip and modules) and/or in code for FPGA or microcontrollers/microprocessors. The role of hardware engineers is still important, because of PCB layout and BOMs, but from the hardware design point of view is almost all already done, just pick a component, read the datasheet and copy the reference design. I’m simplifying, I know, finding the right component is not easy at all, but it seems the hardware engineer role is just reduced to searching and connecting modules. Only IC designers delve into the complexity of hardware design. Do you agree with me or can you explain why I’m wrong, please?

My question arises because I’m considering whether or not to move to hardware design from firmware. Currently, I’ve a master's in Electronic Engineering but I’m working as a firmware designer for microcontrollers."

  • Sign in to reply
  • Cancel
  • dang74
    dang74 over 2 years ago in reply to dougw

    Very interesting.  I wonder if that's a reflection of the cost of technology.  At one time it was quite an investment to put a system together, so yeah you'd want to get 20 plus years out of those early 60s computers.  As time went by things got cheaper, so you start to see more and more upgrades and overhauls.  So when I started we were in an 'out with the old, in with the new' era.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to dang74

    I had some of the opposite experience initially. The place I started at had an IBM1620 (designed around 1959) that used core memory. I also got to work on some ships that had computers designed in the early 1960's - they used drum memory for everything including the system clock, which was just one track on the drum.. On the other hand the pace of innovation has been accelerating since then. A lot of what we take for granted today was considered impossible when I graduated and a lot more would have simply not been conceived of yet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 2 years ago

    "Is electronic engineering dead?" is a lament not unlike "everything has already been invented."  Truth be told I've been guilty of the later, especially back when I was young and was trying to prove myself.  If you study something technical some of what you learned is already out of date by the time you've graduated, and that can be jarring.  In my case when I started working I initially had feelings of regret and I wished I had worked in a different era that was more representative of my schooling.  Eventually though you adapt and find meaningful and rewarding experiences in your work.

    And no, I don't believe electronic engineering is dead.  If you someone is interested in a hardware focused career, they should go for it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago

    We are not yet at a point where electronic design can be done by an AI. It is true that there are a vast number of designs that have been developed already, and these can pretty much be duplicated without electronic engineers, but the number of new and unique electronic designs that have not been designed yet is a much larger number.

    It is also true that electronic engineers will use reference designs and previously developed IP in new designs, but this just avoids having to reinvent the wheel and provides more time to spend developing new IP.

    AI is developing at an accelerating rate so it is very hard to predict when it will become sentient enough to translate any need or desire into a complete solution.

    The question of whether to specialize in hardware versus firmware is more about personal preferences - both are still in high demand and both may give way to AI eventually. I suspect one hardware engineer could keep many more than one software engineer busy so maybe more software engineers are needed.

    The overarching question of deciding what the needs are, is another tricky topic. I doubt people will want to give these decisions away to an AI because it represents giving away power.

    It may seem like designs published on the internet are mostly derivative, but that is because commercially important designs that have lots of new IP, would not be published on the internet. Many of them are too secret to even risk applying for patents.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago

    I don't think it's dead. I think that the popularity of Arduino and other platforms made electronics a lot more accessible, and this has created a huge market for "ready-made" modules and prototyping platforms that are either code-based or sometimes even "zero code". As you mention it's easy now to build stuff just connecting modules together, and if you use Arduino or Raspberry Pi you will probably also find example code and libraries on the internet, so it's just connecting stuff and modifying some lines of code.

    BUT, that's not how real products (i.e: devices expected to be mass produced, certified, and put on the shelves) are designed. Those are still built from the ground up.
    I use modules to prototype and test, but that's never how I intend to build things.


    And even if we were to move into a future where *everything* is just made of modules, someone has to design those modules : )

    Regarding "reading the datasheet and copying the reference design". That has always been the starting point of any application, in my experience, but never the whole final product.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy over 2 years ago

    Electronic Engineering has been iterated in many ways.

    One reason is the advancements in chip designs and availability of SoC, SIP etc that comes with everything that is needed. Consider a timer IC 555. we used to create timer and comparator circuits using this IC in the past but nowadays it is not that much required to do so as integrated chips such as microcontollers or processors will handle the tasks more efficiently. And there could be many such examples for us.

    This does not necessary mean that "EE" is dead. But the number of jobs in circuit design and analog electronics should surely have reduced. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    If you can't have a better product if everyone is implementing the same thing from datasheets, then it's a little hard for firms to innovate. Apple would cease to exist, and we would be buying phones from Alba or Amstrad.

    Each time more performance/features are required, then you need to insert engineers.

    You can tell that some student or person completely removed from the world of engineering work has asked this question.

    It reminds me of one of my first jobs and my desk was piled high with ring binders full of ITU and ANSI docs, and a non-tech friend asked what it was all about. I mentioned that they explained how the phone system worked, so that I could design bits of it. The response I got was, why is all that needed to explain that you just need to lift the phone and dial?


    There are whole TV comedy series' dedicated to this type of thing : )

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller over 2 years ago in reply to robogary

    I suspect that AI will be used as a productivity enhancement tool for EEs for a fairly long period before completely replacing EEs, long enough to have a good career if that's what's needed. However, the demand for EEs will also consequently decrease. One has to be flexible enough to learn not just the specifics of a particular technology as practiced today, but the overriding meta-rules that can be applied outside of one's primary educational focus.

    AI will have customers whenever something is very expensive. NRE for small board runs is less likely to get heavy AI treatment than RE, management, and tasks that require extensive interaction with large portions of the environment that cannot be easily modeled.

    Remember "computer" used to be a job title.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • davebullockmbe
    davebullockmbe over 2 years ago in reply to obones

    Well you have to use the chips that are available of course but its the careful development of the rest of the design that mitigates these safety issues. That's the challenge and skill of being a development engineer I guess. Yes I would lie in bed pondering these issues but still couldn't wait to get to work the next day. Pretty sad aren't I?

    Daveb

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 2 years ago in reply to davebullockmbe

    Out of curiosity, how do you chose the ICs, chips... to use in such medical devices?
    In most datasheet that I have read over the years, there is always a text saying "this device is not for human health, we won't be liable for any injuries/death..." even for the littlest component.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>