Products
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
Member's Forum How to control a remote using a smart phone
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 627 subscribers
  • Views 4240 views
  • Users 0 members are here
  • remote monitoring and control
  • Smart Phone
Related

How to control a remote using a smart phone

colporteur
colporteur over 2 years ago

image

I am looking for suggestions from E14 community members on how to control a remote using a smart phone.

I'm confident someone here has attempted this and actually got it working. I want to use that knowledge. I've combed the internet and found a number of solutions. I want to avoid the rabbit warrens of getting them to work. I'm looking to leverage the community knowledge because you have done it.

The project premise is to connect a smart phone to a controller that actions a remote. My starting point is: how to turn the remote on and off using the smart phone. I use smart phone because I want to keep it broad. It might be an Android or an iphone. I have the latter but my wife has the other. The controller technology is open. I am hoping to use an Arduino of some sort but a single board computer is not out of the solution. The remote in this example is an on/off but maybe it can provide feedback.

This project is for personal use and not to develop a commercial product. There is a limited budget. I'm looking for a cost effective solution not necessarily the cheapest solution. My knowledge level in phone communication is limited. In my project more than one person will be connecting. I've never create a phone app and really don't want to go there. What is simple way of accomplishing that with a phone. I'm not a programmer by training. I've have some skills but would never label myself a programmer.

I'm looking to build a simple solution on the workbench and maybe learn some stuff along the way. I'm looking for suggestions that you know works. Either you have done it yourself or have seen it done and know it works. 

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 2 years ago

    Hi Sean,

    A few more questions:

    (1) Is your garage within coverage of your home WiFi?

    (2) Is the smartphone expected to be within coverage of your home WiFi when controlling the garage door?

    (3) Is the smartphone expected to be a short distance (say 10 meters or less) when controlling the garage door? If longer than 10 meters, what is the maximum expected distance?

    (4) Will the smartphone user be inside their vehicle when controlling the garage door, or does the user expect to be able to control from the smarrphone regardless of whether they are in their vehicle or not?

    The reason for questions 1-3 is that if a long operational distance is required, then that may need either a cloud service, or (worse) messing about with the home router to open up ports (never recommended).

    The reason for question 4 is to see if additional hardware (e.g. transmitter) within the car could be an option (controlled by smartphone).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to shabaz

    1) Yes.

    2) Yes

    3) Yes

    4) Yes

    I have a garage door that provides access to a number of farm vehicles. Vehicles are in and out of the garage daily, Many times with different drivers. The garage/office has wifi. I was thinking maybe an app on drivers phones would give them access to the garage door opener.

    If the solution worked in one garage their are others that would benefit.

    I have little experience outside a computer networks. I was thinking bluetooth to an Arduino that supports it would give me the conductivity from the driver. Just not sure of the phone end. I started to look at iRobbie and thought I don't want to spend a whole lot of time developing. Thumb the phone app and trigger the door through a bluetooth connection seemed a simple idea. How difficult is the phone part?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to colporteur

    Hm, that's suddenly increased the complexity greatly, when you mention that many different drivers need access. The complexity will depend on how much security is required.

    Your need is actually a complete solution, providing secure access to many users. I think it's too ambitious to want to develop this from scratch unless familiar with the technologies.

    It's not the same as just remotely controlling a device from a phone for a few select trusted friends or family.

    There may be ready-made offerings, I'm not aware of them, so if you were completely set on doing it DIY-style:

    Originally, I was going to suggest something like Pi Pico could be used, since it has both Bluetooth and WiFi, and it would be quite straightforward to have a simple page that works on Android and iPhone, to communicate over BLE or WiFi depending on what's preferred.

    But, since more security is needed, then probably a Raspberry Pi or similar is required, to at least log when people open/close the door. Users could be required to authenticate with a password, but then that may entail sending and receiving data (not just a simple transmission), plus writing some JavaScript at a minimum, so it's no longer a quick thing to implement. Still feasible though, but not a quick thing, it would need software development.

    If you want a basic minimum viable product that would have the flexibility for implementing some form of authentication or using rolling codes or whatever, but initially would just be a very basic not very secure method until more code was written, then you could use a Raspberry Pi, running code that makes it operate as a 'BLE Peripheral', perhaps waiting for a passcode (and locking for a minute if the wrong passcode is entered) and connected via GPIO to your remote control (e.g. using a relay). 

    At the mobile end, you'd need to write a single HTML file that makes the phone connect via BLE (the most basic thing could be for the user to type say a 4-digit passcode that is hard-coded on the Pi).

    The HTML file could either be e-mailed to the people that require access, or could be placed on the Internet (it would be useless to those who are unauthorized, since they would not have the passcode).

    The above is not very secure, but none of the hardware would need to be swapped out to make it more secure; simply, the code would need to be developed.

    As you can see, there's still a lot to learn if you're new to this. To use a Raspberry Pi as a BLE Peripheral, the search term is 'node.js Bleno' for one method of doing it (there are other ways too). To write a HTML file with some JavaScript to communicate using BLE, the search term is 'Web Bluetooth API'.

    All the above could be eliminated if there's any ready-made solution, but I don't know of one, hence there's all the coding effort.

    Personally, I think it's best to simply place a keypad near the garage door, make users type a code, and you could change the code periodically, That's still low-security, but way simpler to do, using any Arduino and waterproof keypad. If you use say a Pi Pico for that, then you could set the code over WiFi, that would be quite easy.

    .

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to BigG

    I was naive to think there would be a simple solution. I like   dougw video listing. The phone part is what keeps me at bay. I haven't dabbled with them. Having a working solution and not bare metal start is what I was looking for. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 2 years ago in reply to colporteur

    If you treat this like fishing you'll have no bother catching the big one. It starts by choosing the right fly (product) and then spending a bit of time attaching it to the hook (putting the hardware together). Then let your technique and experience do the rest when standing chest deep in water... and, as I'm sure you know, this means having multiple flies in the bag... as the first one you choose might not be the best one.

    Just take little steps and take your time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 2 years ago in reply to colporteur

    If you treat this like fishing you'll have no bother catching the big one. It starts by choosing the right fly (product) and then spending a bit of time attaching it to the hook (putting the hardware together). Then let your technique and experience do the rest when standing chest deep in water... and, as I'm sure you know, this means having multiple flies in the bag... as the first one you choose might not be the best one.

    Just take little steps and take your time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 2 years ago in reply to BigG

    I was naive to think there would be a simple solution. I like   dougw video listing. The phone part is what keeps me at bay. I haven't dabbled with them. Having a working solution and not bare metal start is what I was looking for.