Member's Forum Hi everyone!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 625 subscribers
  • Views 2542 views
  • Users 0 members are here
Related

Hi everyone!

JoRatcliffe
JoRatcliffe over 2 years ago

Hi everybody, I've joined the team behind the element14 community and I just wanted to say a quick hello.

I have an important project right now which is helping make webinars, on-demand videos, challenges and the site as a whole be the best that they can be. I'm eager to to help this community continue to be an informative, enriching and entertaining(!) place to be.

Less importantly perhaps I am also experimenting at home with smart lightbulbs and motion sensors currently. A hallway where people are coming and going seems like a natural use case but I want to see if I can get one working in another area like the kitchen where I'm sometimes not spending a lot of time (eg. making a coffee) but I'm also not moving around a lot (eg. standing in front of the coffee machine). It's probably just a case of me looking at how long the lights stay on when movement is detected and how often movement is required for continuous light etc, but a fun lil project nonetheless.

  • Sign in to reply
  • Cancel
  • electronicbiker
    electronicbiker over 2 years ago

    Many many years ago I bought a flat electrovoltaic plate from Proops. It was about 1.0" by 1.5", very thin, and with two wires coming from it. Commonly used in garden ornaments these days.

    One evening I connected it to a germanium transistor, probably an OA10 as silicon ones hadn't been invented yet, a U2 cell, and an electric motor of the type used in model boats. In the darkness of my unlit bedroom it did nothing, but when I shone a torch at the light sensor the motor burst into life! This was exciting, I'd only ever built crystal radio sets before. The whole lot was sitting on the top surface of a small wooden chest-of-drawers, and the vibrations of the slightly unbalanced motor echoed a pleasant purring sound throughout the room.

    After a while I disconnected one end of the cell and went downstairs to watch Dr Who. Later, it was bed time. My mother had closed the curtains while I was watching Dr Who from behind the settee, so the room was in darkness. I re-connected the cell with the elastic band, shone the torch at the sensor, and Lo and Behold, it still worked! I don't know why I didn't disconnect the battery again, but i didn't.

    Came the morning, the sun was shining through the tiny holes in the wartime black-out curtains. I was thinking about getting up when mother strode in, told me to get up as it was school today, and opened the curtains...

    The low hum from the motor just behind her scared her so much that she ran screaming from the room, all the way downstairs and into the kitchen. Some of the words that she used were unknown to me, despite me being an avid book reader. I was not the most popular of her offspring for several days, although my father was intrigued.

    So be careful joratcliffe, you never know how people will react to modern technology!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JoRatcliffe
    JoRatcliffe over 2 years ago in reply to beacon_dave

    That is fantastic inspo, thank you! I've gone with Philips Hue too so this is perfect. I'm really looking forward to meeting Natasha and the other presenters as soon as I can.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • md_steve
    md_steve over 2 years ago in reply to kmikemoo

    Bummer. It's a shame these decisions are always made by someone that's too high up to see individual circumstances and adjust for ground truths.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to md_steve

     md_steve I don't think our occupancy sensors are so cool as to have an app.  My guess is that they are simple PIR sensors.  For one building, I should probably look a little harder for the lighting control center.  For another, I know that they are individual lights with integrated sensors.  No app for those as the guy that installed them also dislikes the "feature". If it had an app, he'd be using it.
    (Auto-OFF after a set time is a county mandate.  We have to have these types of lights in any space the county classifies as primarily a warehouse.  Regretably, it's also our repair bay.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    Welcome to element14, I look forward to working with you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 2 years ago

    Welcome to the club! Great to meet you Smiley  

    Good luck with the sensors and lights, I’m hoping you’ll share the journey! I tried a hallway sensor/light thing several years ago but gave up because the software was too limited to handle the automatic-off bit, and it couldn’t tell whether I was coming home or leaving Shrug So now I just ask Alexa to turn them on or off when I need it Smiley 

     -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • md_steve
    md_steve over 2 years ago in reply to kmikemoo

    Our building was recently upgraded with occupancy sensors in every room and hallway. I use small task lights over my bench and desk instead of  the overhead lights. As soon as I open my door the overhead lights would come on. Fortunately they are programable so the first thing I did was download their app on my phone and set the sensor to "Manual". It still pops on once in a while (line noise?)  but mostly my overheads are off all the time. The opposite might work for you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago

    JoRatcliffe Welcome to the Community.  Good luck on your project.  We have something like what you describe in a couple of our warehouses and I despise them.  The lights turn themselves off while I'm working on a piece of equipment.  Very annoying. Laughing

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 2 years ago

     JoRatcliffe Welcome to the Office, The problem with things that are 'Smart' is they cost way too much. In my project SmartHab I looked at it very differently. As I already have two fobs one is short-range and the other is long-range RFID, For your hallway I would use long-range RFID, depending on the length to the hall you might need two of them. or ie near the doors, so you can use two in a long hall one reader near each entrance or exit.  so basically when one of the sensors sees a tag it turns on the lights when the other sensor sees the tag the lights will go off!  so the problem arises when you have a hallway going to a few bedrooms,  again the same game is played with the sensors. easy-peasy lemon squeezy! ~~Cris. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dwinhold
    dwinhold over 2 years ago

    Welcome to the community!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>