Member's Forum Air Band Receiver High Sensitivity Aviation Radio 118-136MHz AM DIY Kit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 626 subscribers
  • Views 7781 views
  • Users 0 members are here
Related

Air Band Receiver High Sensitivity Aviation Radio 118-136MHz AM DIY Kit

scottiebabe
scottiebabe over 2 years ago

A 30 year-old electronics hobby kit still lives on to this day.

I came across a superhet airband receiver kit that peaked my interests. It’s based on a few venerable but not extinct radio ICs, namely the NE602 and the MC1350. I don’t know where the kit producer is sourcing these ICs, but for $20 it was worth taking a chance on it being more than a pack a of bubblegum. Fingers crossed I receive at least functional equivalent ICs, if not new/salvaged old stock.

image

 imageimage

You can find the kit at the usual places searching “Air Band Receiver High Sensitivity Aviation Radio 118-136MHz AM DIY Kit”

The schematic is to clean and logical to be a typical noname solder kit. After some digging around on the internet, I found the origin of the kit. This project was originally designed by Fred Blechman and published in the spring 1994 issue of "Electronics Hobbyist Handbook" by Gernsback Publications.

A pdf of the publication is available here:

image

https://www.worldradiohistory.com/Archive-Poptronics/Experimenters-Handbook/Electronic-Hobbyist-Handbook-1994-Spring.pdf (Page 82)

Tony van Roon also shares their experience and analysis of the project kit here:

https://www.learningelectronics.net/VA3AVR/circ/aviarx/aviarx.html

  • Sign in to reply
  • Cancel
  • Mattia.Zamana
    Mattia.Zamana over 1 year ago

    This Arrow double down️ is how I made it. I'm really happy with the aesthetic result and the receiver works really well.

    https://youtu.be/s0W8N2rxZcE?si=ZyAJDXZWBiyXQrJD

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • dan.corneanu
    dan.corneanu over 1 year ago in reply to scottiebabe

    Hey,

    I've just received mine and I think that the NE602 is faulty because it does not oscillate.

    It's obvious it has been harvested from another board and it has some signs of abuse.
    However, before I throw away the IC and try to source another one, any suggestions on how I could prove that the IC is indeed the culprit?

    Regards,

    Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nobcha
    nobcha over 2 years ago in reply to scottiebabe

    Hi, I have ever assembled these kits. It's cheap but very nice, when you improve some.PCB inductors are bad.

    Please refer my report of "I studied how to tune PCB pattern type filter".
    nobcha23.hatenadiary.com/.../174051

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to Jan Cumps

    LOL dave is the best! Adjusting a one-turn pot to 0.1% of its full scale range will require some tongue work...

    If the rxcv has 10 kHz IF bandwidth and 14 MHz tuning range.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe
    scottiebabe said:
    while twiddling the tuning pot

    Did you have your tongue in the right angle?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago

    The front-end preselect filter is OK, it has some insertion loss and not a whole lot of rejection in the FM broadcast band. Could it be better, possibly, but it's not a showstopper.

    imageimage

    The local oscillator created with the NE602 is alive and well.

    image

    The tuning potentiometer varactor tunes the LO from 130.7MHZ to 145 MHz (left my SA in max hold while twiddling the tuning pot)

    image

    So far it would appear as though I got a real NE602 Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    Looks like you can have some fun with it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to colporteur

    In this case the designer didn't capture the PCB inductor as circuit component and just "winged" it with PCB traces.

    How PCB artwork is drawn at a schematic level isn't quite as rigidly defined. Here's an LNB example 

    image

    image

    https://www.nxp.com/docs/en/application-note/AN11674.pdf 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to scottiebabe

    Is the symbol they used in the schematic for a planar inductor a standard? I can't seem to find a reference. I see on the schematic page they have the symbol off to the right side with some Chinese script. I assume it is indicating this is how we draw a planar inductor

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to dwinhold
    dwinhold said:
    Trying to get the younger generation into it is so hard.

    How are you trying to sell it to them though ? The younger generation are communicating wirelessly via text messaging every day with ease, so learning Morse Code probably isn't going to be the way to promote it. It perhaps could do with reinventing itself a bit given the ease of access to alternative wireless communications technology in the modern world.

    This probably applies to a lot of hobbies these days however.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>