Member's Forum How do you make reliable, low-cost cables quickly?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 52 replies
  • Subscribers 624 subscribers
  • Views 6059 views
  • Users 0 members are here
  • dougw
  • bootlace connectors
  • custom cables
  • MTA
  • Yodamonk
Related

How do you make reliable, low-cost cables quickly?

dougw
dougw over 2 years ago

I do lots of electronics design and building and inevitably need to make lots of cables. Since making cables is not my favorite activity, I try to use methods that are quick while still providing reliable connections. And of course I always need to keep the costs down.

This short post shows a couple of the main ways I accomplish these objectives.

image

Yodamonk, the cable guru.

Custom Cable Methods

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

I haven't posted much content lately so I thought I would post something about making cables. This activity is not usually exciting enough to be a great blogging topic, but I also wanted to play around a bit with some AI media generation. (No AI text though) The tough Yodamonk dude came out amazing.

I am always looking for efficient ways to make useful cables, so if you have any interesting tips, please jot them down below...

  • Sign in to reply
  • Cancel
Parents
  • genebren
    genebren over 2 years ago

    I really like to use the crimp ferrules on wires that are getting inserted into screw terminals.  And old AMP IDC connectors are really nice, even if I don't have your fancy gun, only the T-handle tool (which is not so easy to use).

    image

    Thanks for sharing your thoughts on cables.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to genebren

    Once you try crimp ferrules (bootlace connectors) it is tough to go back. I am still looking for a good source (read cheap) that are simple metal tubes - no plastic sleeve.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to dougw

    I have a bunch of these and they’re very useful. In fact, I had to dig them out to help with a 3D Printer I’m in the middle of building.

    They are also useful as test points on a board, at least with through holes but I’ve not tried soldering one to a pad.  If you push it through the hole on the PCB, the flange will stop it falling through and your probe end will slot neatly inside and be held freeing a hand up.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • electronicbiker
    electronicbiker over 2 years ago in reply to Andrew J

    I try not to use these whenever there is just a hole and a pad on one side of the PCB, as oppose to a plated-through-hole with a pad on both sides of the PCB. Especially if you intend to use it as a test point as well as the mechanical support for a ferrule. Using them as the support for set-on-test components is even more critical as they may have to have components soldered, removed, and soldered again several times before the correct value is achieved. I have found that Vero-pins work well, the ones that look like a small nail that has been knurled from underneath the head to about half-way down its length. They are a tight fit in both fibre-glass and paxolin so I usually fit them first before any of the other components, especially if the PCB is tightly packed. The ones I have used are not hollow; they are too small to be drilled. The hollow ones tend to be thicker and so occupy a lot of real-estate.

    If there is a pad on both sides of the board then use both of them, and solder as quickly as possible. Excess heat can make the holes in the PCB a loose fit and/or cause the pads and nearby track to come unstuck. Using the holes through the ferrules to support probes requires well-fitted ferrules! 

    There is another type; they have a pair of 'jaws' at the top. Two of them will hold small components for soldering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • electronicbiker
    electronicbiker over 2 years ago in reply to Andrew J

    I try not to use these whenever there is just a hole and a pad on one side of the PCB, as oppose to a plated-through-hole with a pad on both sides of the PCB. Especially if you intend to use it as a test point as well as the mechanical support for a ferrule. Using them as the support for set-on-test components is even more critical as they may have to have components soldered, removed, and soldered again several times before the correct value is achieved. I have found that Vero-pins work well, the ones that look like a small nail that has been knurled from underneath the head to about half-way down its length. They are a tight fit in both fibre-glass and paxolin so I usually fit them first before any of the other components, especially if the PCB is tightly packed. The ones I have used are not hollow; they are too small to be drilled. The hollow ones tend to be thicker and so occupy a lot of real-estate.

    If there is a pad on both sides of the board then use both of them, and solder as quickly as possible. Excess heat can make the holes in the PCB a loose fit and/or cause the pads and nearby track to come unstuck. Using the holes through the ferrules to support probes requires well-fitted ferrules! 

    There is another type; they have a pair of 'jaws' at the top. Two of them will hold small components for soldering.