Member's Forum What're you up to this weekend?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 55 replies
  • Subscribers 628 subscribers
  • Views 4828 views
  • Users 0 members are here
  • weekend plans
Related

What're you up to this weekend?

cstanton
cstanton over 2 years ago

I'm going to tinker with different soundcards I have, USB and PCI to see which is better at storing and playing audio from old vinyl records that I have.

What do/don't you have planned?

  • Sign in to reply
  • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to Jan Cumps

    Typical ChatGPT non-intelligence.

    The chip in the neopixel probably uses 40nM geometry, the light guide is a plastic moulding , single homogenous material (acrylic) etc etc.

    There's a good video on you tube of a neo pixel factory which shows the parts going through multiple stages of automatic assembly and test.

    I suspect that the main issue is that the low volume market for light guides is small. I'm sure they will get pretty cheap if you want enough - but when something cost less than a penny each you need to shift a lot in a day to make a living !

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Jan Cumps

    I asked chatgpt.

    "how comes that light pipes for neopixels are more expensive than neopixels themselves?"

    In essence, while Neopixels themselves are low-cost due to mass production and simple components, light pipes require specialized materials, precision manufacturing, and are often customized for specific applications, all of which contribute to their higher cost.

    There's a longer analysis that I can post if interested.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz
    shabaz said:
    I've never understood why the light pipes cost so much more than the LEDs themselves!

    I'd turn it around. How comes the pixels sell cheaper than the pipes? I think it's based on volume. Pixels are produced in such high volumes, in a competitive market, that it drives the price down.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 1 year ago in reply to DAB

    How did they come out? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago in reply to kmikemoo

    Frowning2 Got to everything but the Opta.  Tended to the family graves.  Chatted with an old Army buddy.  Coached an old friend through some depression.

    REALLY glad right now that I didn't get selected for the Opta RoadTest! JoyThumbsup  Truth.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to michaelkellett

    I've never understood why the light pipes cost so much more than the LEDs themselves! Given that they are approximately the same thing, and one is missing the LED die and leads.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago

    I want to use multicoloured LEDs as indicators on an instrument front panel and It will need 32 of them. I thought I might use the 2mm square neopixels and I bought 1000 from Aliexpress for about 1.6p (£0.016) each.

    I thought I had better see how well they worked.

    I'm driving them from the SPI MOSI pin on an ARM processor (Giga Devices GD32E103 and I had to tweak the clock to get a good ratio of high and low times from 4 bits of a 16 bit SPI data word.

    Right now the code is using interrupts (one for every 16 bit word transmitted) but I'll change it to use DMA.

    Happy to post the code if any one wants to play with it. The GD processor SPI is a pretty much exact clone of earlier ST  ST3210x processors.

    I set up a pseudo random thing to drive it (sorry about the kitchen paper optical filter - the camera couldn't cope with bright LEDs).

    So I'm pleased to say that the sub 2p neopixels work OK.

    Unfortunately the little light pipes (plastic rods a few mm long with a domed end) cost about 5x as much as the pixels - but I need them to get the light through the front panel.

    image

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to Jan Cumps

    Probably not, he was a nice chap.  Been making swords for 45 years now; it was absolutely fascinating.  He collects his own rocks to grind out the iron sand, then turns that into clumps of rough metal which he then chips off bits to heat up to turn into an ever expanding block, which he is able to fold over itself.  Really skilled stuff. Legally, he can only make 2 a month so he supplements with knives and other edged implements like branch cutters.  Sharp doesn’t cover it!

    And yes, hand tools works!  He made something akin to the cutlass in the link but more cleaver-like:  made mincemeat out of a wooden block.  He gifted my wife and I a knife each which I think I’ll treasure rather than use.  Amazing bloke.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to Andrew J

    I guess we could classify that one under the heading of 'hand tools' ?

    Large bladed items are starting to prove popular on here:

    /technologies/test-and-measurement/w/documents/28264/the-rough-rugged-and-covered-in-mud-wishlist?CommentId=f341ad34-807b-4f5b-b88d-ad9f3442d152

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Andrew J

    The guy from Kill Bill?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<>