Member's Forum I like how this sounds, but then again, I probably wouldn't
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 593 subscribers
  • Views 2756 views
  • Users 0 members are here
  • audio compression
  • cassette tape
  • mp3 to cassette tape
Related

I like how this sounds, but then again, I probably wouldn't

stanto
stanto over 1 year ago

It's 3:30am and I've finished fighting with the Baldur's Gate 3 toolkit to edit a mod I'm working on, and a thought hits me.

Wouldn't it be funny to store music on a cassette?

No, not like that.

I'm talking about, digital music. Take say, an MP3 or equivalent, potentially lossy compression audio format - because it would be funnier. Then create an audio file at a low bitrate, depth and frequency. Then have write it to a cassette tape, like in the ZX Spectrum / Commodore 64 days.

Then play it back and decode it on the fly!

I believe it would be an interesting juxtaposition of technology while being a challenge to get the most out of the compression and data rates, and handling errors on the way. Resulting in a pretty hilarious audio file.

Consider it an art piece.

I wonder what the bill of materials would look like for that? I still have some as-new cassettes lying around...

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 1 year ago +7
    If you want an idea of the circuitry that was originally used in these kind of interfaces, this is a cassette tape interface I built around 1979. I think it might have been based on a Don Lancaster design…
  • jc2048
    jc2048 over 1 year ago in reply to jc2048 +4
    He included the 'Bit Boffer' in his TV Typewriter Cookbook. So that's where I came across it. Would it work if stanto simply took the analogue bits (with maybe an actual comparator on the input to the…
  • shabaz
    shabaz over 1 year ago +2
    BoM could be as low as a sound card and a PC, or a Raspberry Pi (assuming a cassette recorder/player already exists). There are codecs like FreeDV which have a chance to be usable if you're looking for…
Parents
  • shabaz
    shabaz over 1 year ago

    BoM could be as low as a sound card and a PC, or a Raspberry Pi (assuming a cassette recorder/player already exists). There are codecs like FreeDV which have a chance to be usable if you're looking for real-time playback on-the-fly (i.e. not buffering up a load of data over a longer time, and then playing out over a shorter time). But whether such codecs play nicely with tape (which will have slight speed and frequency deviations (wow/flutter) probably is for further study, since those codecs were not designed for tape. It won't sound very great (and they are more intended for speech, so the music will sound bad with such a codec), but perhaps if non-standard things were done (e.g. record at a higher tape speed, or use many tracks on the tape, etc., then that could help perhaps.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 1 year ago

    BoM could be as low as a sound card and a PC, or a Raspberry Pi (assuming a cassette recorder/player already exists). There are codecs like FreeDV which have a chance to be usable if you're looking for real-time playback on-the-fly (i.e. not buffering up a load of data over a longer time, and then playing out over a shorter time). But whether such codecs play nicely with tape (which will have slight speed and frequency deviations (wow/flutter) probably is for further study, since those codecs were not designed for tape. It won't sound very great (and they are more intended for speech, so the music will sound bad with such a codec), but perhaps if non-standard things were done (e.g. record at a higher tape speed, or use many tracks on the tape, etc., then that could help perhaps.

    • Cancel
    • Vote Up +2 Vote Down