Member's Forum I like how this sounds, but then again, I probably wouldn't
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 626 subscribers
  • Views 3387 views
  • Users 0 members are here
  • audio compression
  • cassette tape
  • mp3 to cassette tape
Related

I like how this sounds, but then again, I probably wouldn't

stanto
stanto over 1 year ago

It's 3:30am and I've finished fighting with the Baldur's Gate 3 toolkit to edit a mod I'm working on, and a thought hits me.

Wouldn't it be funny to store music on a cassette?

No, not like that.

I'm talking about, digital music. Take say, an MP3 or equivalent, potentially lossy compression audio format - because it would be funnier. Then create an audio file at a low bitrate, depth and frequency. Then have write it to a cassette tape, like in the ZX Spectrum / Commodore 64 days.

Then play it back and decode it on the fly!

I believe it would be an interesting juxtaposition of technology while being a challenge to get the most out of the compression and data rates, and handling errors on the way. Resulting in a pretty hilarious audio file.

Consider it an art piece.

I wonder what the bill of materials would look like for that? I still have some as-new cassettes lying around...

  • Sign in to reply
  • Cancel
Parents
  • battlecoder
    battlecoder over 1 year ago

    I did some experiments on digital data storage on cassettes a couple of years ago. Whatever the kind of data you want to store (compressed music, raw samples, etc) keep in mind that you are going to have a VERY low bitrate.

    You can look into how digital data is normally stored in cassettes, and you'll find that they pick a frequency to represent "1" and one to represent "0". You would normally read at least 4 cycles at the slowest frequency to detect a one or zero, so your "baud rate" will be limited by how fast it would be to read 4 cycles of the slowest frequency you select.

    Due to the frequency response of the magnetic substrate, a tape can't record anything above 16 KHz or thereabouts. And at that limit you are already getting a severely attenuated wave that will be hard to tell apart from noise. There are fancier, more expensive tapes with better frequency response, but the average tape was very limited.  So let's say you select 12KHz for "1", and 6 KHz for "zero" (which is already kinda pushing it).

    Because you need 4 cycles of the lowest frequency (traditionally at least; you could try to get away with using less cycles), your highest baud rate in this scenario would be 6000/4 = 1500 bits per second. And that is without considering adding error correcting bits, or start/stop bits, etc.

    Most computers from the 80s that used tapes would use lower frequencies (1.2KHz or 2.4 KHz at most, probably for reliability and to avoid getting close to the point where the tape starts attenuating the wave) and would end up with a baud rate of like 300 bits per second. 600 baud was fast, and 1200 baud was pretty much "turbo".

    If I were you, I'd start by trying to figure out a format/compression that would allow me to represent a song at those low bitrates and check how that sounds, while finding a way to convert "normal" songs to that.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to battlecoder

    There is a good article on theis subject (almost) on Wikipedia:

    https://en.wikipedia.org/wiki/Modem

    It explains how you can get up to 56000 bits per second over a telephone quality audio channel.

    I don't think that anyone ever optimised a codec for audio cassette data recording but since you can get 12kHz audio bandwidth and better than 45dB signal to noise ratio I would guess that  better than 100kbit/s is possible.

    There is an article here

    https://electronics.stackexchange.com/questions/596747/how-much-data-could-be-stored-on-a-standard-compact-cassette-using-modern-encodi

    which discusses the subject froma  different point of view and concludes a (probably) lower rate.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 1 year ago in reply to michaelkellett

    I've not read through the specifics of standard yet, but from a quick glance to the wiki description I assume they were using the amplitude of the wave as well as part of the encoding. Now, I'd assume that at that point encoding the data starts  becoming a lot harder

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • battlecoder
    battlecoder over 1 year ago in reply to michaelkellett

    I've not read through the specifics of standard yet, but from a quick glance to the wiki description I assume they were using the amplitude of the wave as well as part of the encoding. Now, I'd assume that at that point encoding the data starts  becoming a lot harder