Member's Forum I like how this sounds, but then again, I probably wouldn't
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 626 subscribers
  • Views 3383 views
  • Users 0 members are here
  • audio compression
  • cassette tape
  • mp3 to cassette tape
Related

I like how this sounds, but then again, I probably wouldn't

stanto
stanto over 1 year ago

It's 3:30am and I've finished fighting with the Baldur's Gate 3 toolkit to edit a mod I'm working on, and a thought hits me.

Wouldn't it be funny to store music on a cassette?

No, not like that.

I'm talking about, digital music. Take say, an MP3 or equivalent, potentially lossy compression audio format - because it would be funnier. Then create an audio file at a low bitrate, depth and frequency. Then have write it to a cassette tape, like in the ZX Spectrum / Commodore 64 days.

Then play it back and decode it on the fly!

I believe it would be an interesting juxtaposition of technology while being a challenge to get the most out of the compression and data rates, and handling errors on the way. Resulting in a pretty hilarious audio file.

Consider it an art piece.

I wonder what the bill of materials would look like for that? I still have some as-new cassettes lying around...

  • Sign in to reply
  • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to colporteur

    I threw out the missus Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 1 year ago in reply to jc2048

    You built it in 1979, I just finished high school and you still have the book. Impressive or horder, not sure on that? Actually I know I still have my college text books from that year. My missus keeps asking me to throw them out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 1 year ago in reply to jc2048

    He included the 'Bit Boffer' in his TV Typewriter Cookbook. So that's where I came across it.

    image
    Would it work if stanto  simply took the analogue bits (with maybe an actual comparator on the input to the receiver, rather than using the 3130 op amp) and attached them to a Pico? Could the PIOs emulate what the CMOS logic is doing and the program emulate the UART? If so, that might be the simplest and cheapest way to do what is being asked for.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 1 year ago in reply to michaelkellett

    I've not read through the specifics of standard yet, but from a quick glance to the wiki description I assume they were using the amplitude of the wave as well as part of the encoding. Now, I'd assume that at that point encoding the data starts  becoming a lot harder

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 1 year ago in reply to scottiebabe

    It's very possible, though I don't now recollect the article. I didn't get to see Byte much until later - the various magazines weren't imported here in the UK very much at that stage, but I did obtain from somewhere the first book where they rolled together a lot of the more interesting content, so perhaps it was from that. I might still have it - I'll have a rummage around later.

    The only US magazine I read regularly was Dr Dobbs, which I had a subscription to for a few years (it got flown over air mail). For a while, that had some really good stuff in it - I can remember rewriting one of the various Tiny BASICs that appeared, from 8080 code to 6502. Indeed that might have been part of my motivation for doing the cassette interface: it would have been painful entering that in machine code every time I wanted to use it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 1 year ago in reply to jc2048

    jc2048 Thank you for the reference, I believe you are referring to Don Lancaster’s “Bit Boffer”

    www.tinaja.com/.../bitboff.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • electronicbiker
    electronicbiker over 1 year ago

    Having read through all the replies so far, I feel you might be interested in 'Packet Radio', a system of data transfer between two computers using a tranceiver each (on the same radio frequency) and a modem usually based around a Z80. Zero's and One's were harmonically-related audio ferqencies. The system would work with several users on each channel, it coped with 'collision detection' and slightly inaccurate baud rates. If more than four zeroes were sent then a system called 'bit-stuffing' was used to insert a One into the data stream to re-align the clocks, which were phase-locked to the incoming signal. The receiver would remove it so that the data was not corrupted. The dual tones were audio frequencies and used the CUTS tape interface on the Beeb. This also selected Transmit or Receive using the relay contacts that normally stopped and started the cassette recorder.

    Reading your contribution made me think that using a similar system you could use multiple recorders to produce Electronic Music based on random mixing of several different cassettes set to playback, simultaneously and/or only one at a time, or any combination of the above. There is an article on Wikipedia that explains it all far better than I can, it must be 40 years since I used packet radio! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 1 year ago

    If you want an idea of the circuitry that was originally used in these kind of interfaces, this is a cassette tape interface I built around 1979. I think it might have been based on a Don Lancaster design. It worked at 300 baud and was quite solid and reliable recording and playing back. The large chip is a UART. The panel switch is labelled play and record. I think that the relay controlled the motion of the tape, somehow, maybe via the small mains PSU I built to power the recorder to save on batteries.

    image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Cquk
    Cquk over 1 year ago

    I guess the first task is to find the tape recorder. From memory you will need to read the file back into memory first before it can be played back. The data rate is very slow. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to battlecoder

    There is a good article on theis subject (almost) on Wikipedia:

    https://en.wikipedia.org/wiki/Modem

    It explains how you can get up to 56000 bits per second over a telephone quality audio channel.

    I don't think that anyone ever optimised a codec for audio cassette data recording but since you can get 12kHz audio bandwidth and better than 45dB signal to noise ratio I would guess that  better than 100kbit/s is possible.

    There is an article here

    https://electronics.stackexchange.com/questions/596747/how-much-data-could-be-stored-on-a-standard-compact-cassette-using-modern-encodi

    which discusses the subject froma  different point of view and concludes a (probably) lower rate.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>