Products
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
Member's Forum Assistance in" Roadmap to Master Embedded Electronics and Register-Level Programming"?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 627 subscribers
  • Views 1266 views
  • Users 0 members are here
Related

Assistance in" Roadmap to Master Embedded Electronics and Register-Level Programming"?

VishalSoni00
VishalSoni00 over 1 year ago

Hi everyone,

I’m Vishal Soni, a Bachelor of Technology student majoring in Internet of Things (IoT). I’m an electronics enthusiast with a strong foundation in PCB design, circuit debugging, and a keen interest in hardware and embedded systems.

I’ve worked on several projects—some designed independently and others built with assistance from tools like ChatGPT. While these experiences have been valuable, I want to dive deeper and gain a strong grasp of register-level programming for microcontrollers. My goal is to understand microcontroller architecture better and work at a lower level of abstraction to build efficient and scalable solutions.

  • Sign in to reply
  • Cancel
  • electronicbiker
    electronicbiker over 1 year ago

    I started with a PIC chip many years ago, having bought a programmer, a manual, and several different chips. The manual is excellent, the programmer still works, and my first program worked after a bit of trial-and-error with the inputs to the A-D interfaces. This was not long after they first came out, they were remarkably cheap in those days!

    The programmer required RS 232 for comms, and I fitted it with a zero-insertion-force socket to plug the PIC in and out as necessary.

    The program I really wanted was to input two analogue voltages controlled by a two-axis analogue joystick, four push-buttons to four digital inputs, and that was it for the hardware. I wrote the software using a simple text editor, it occupied about two screens-full. This device replaced several CMOS up/down counters, two 'discreet' A-D CMOS converters, two pairs of quadrature decoders, and so on. The only thing that didn't work properly the first time I tried it was the joystick because I'd wired both axes back-to-front. Having sorted that out, I could fly my little Tiger Moth with the joystick, just like the real thing. I mean, whoever heard of flying a 'plane with a mouse?

    To make the same device with discreet components and a power supply would have occupied a box about the size of a shoe-box to put it all in. As it is, the PIC version is in a box about the size of a tobacco tin. It plugs into the mouse socket on the Acorn RISC-PC and works a treat. Since then I have made several other PIC-powered devices, I would have used them at work except that work decided they were too new to get any reliable reliability ratings.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to VishalSoni00
    • To a memory address
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • VishalSoni00
    VishalSoni00 over 1 year ago in reply to Jan Cumps

    its like assigning zeroes and ones to port of MCU ,I guess??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to VishalSoni00

    The existing toolchain will be able to handle your assembly files. If your IDE supports it, it 'll most likely assemble source files with extension ".S".

    It's also possible to inline assembly code. (example)

     __asm__ ("movl %eax, %ebx\n\t"
              "movl $56, %esi\n\t"
              "movl %ecx, $label(%edx,%ebx,$4)\n\t"
              "movb %ah, (%ebx)");

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • VishalSoni00
    VishalSoni00 over 1 year ago in reply to dougw

    thanks this helps me a lot 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • VishalSoni00
    VishalSoni00 over 1 year ago in reply to rsc

    Right now, I am writing code for the ESP-IDF for Espressif system boards or ARM controllers. Which assembly code compiler can I use?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 1 year ago

    Try working through one of the many on-line courses on assembly language programming. I would suggest the MSP430 as an MCU that has a nice clean architecture with orthogonal registers. (all registers have the same functionality) This is much simpler to learn the concepts with than something like an ARM chip, where the assembly language got very messy as they grew their functionality.

    Here is an example course:

    https://www.youtube.com/watch?v=9MmKNUemEJw

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 1 year ago

    Pick a micro, AVR, PIC, Intel, etc. Then get an ISP or JTAG programming board depending on what you need to program the micro.  Install the required programming toolchain and go for it.  If you really want to learn the nitty gritty details of a micro, use an assembly code compiler.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • VishalSoni00
    VishalSoni00 over 1 year ago

    can anyone suggest me a road map for register level programming