Hello Friends,
Let me share this repository with you:
Fully open reproduction of DeepSeek R1
https://github.com/huggingface/open-r1
Perhaps, you can make something new out of it.
Hello Friends,
Let me share this repository with you:
Fully open reproduction of DeepSeek R1
https://github.com/huggingface/open-r1
Perhaps, you can make something new out of it.
While I think that DeepSeek will have an impact, it's going to be on par with other advancements in the field that already were great on their own (for example: Llama), I agree with the sentiment that it's not going to be as dramatic as people are making it to be. It's absolutely astounding work, for sure, but it's not "David defeating Goliath". Sadly every new thing is reported as an Earth-shattering event with world-changing consequences that will absolutely change life as we know it. That's always a lie, and that's what gets the panic going and people (and markets) overreacting.
And talking about blowing things out of proportion, I would also love if companies would start being more realistic with how they present the models. They are good as text manipulation tools that seem to hold some amount of knowledge and concept abstractions. They are good at extracting core ideas, commands or actions from natural language, executing on them, and then reporting back in somewhat-natural language, so they are great for personal assistants and text-processing aids. But that's not how they "sell" them. They advertise them as if they were a cosmic all-knowing thing that will "boost" productivity and reduce the workload of people everywhere, and that's absolutely not even near to being a reality.
Now, back to DeepSeek. For models to be profitable and actually useful without becoming a major disaster both financially and environmentally, they need to start using less resources, and that's exactly where DeepSeek presents a move in the right direction. The fact that people can download it from a repo (thanks for sharing one that seems to streamline some of the process) and run it without requiring too expensive hardware, will hopefully mean that more and more people will be able to play with this kind of tool and maybe find a better use for it than replacing customer support on their products and then finding out in court that it wasn't a great idea.
I heard from other post/forum about this comparison:
Other USA counterparts use 100% resource to achieve a certain result while Deepseek uses only 5% resource to achieve the same result.
Assuming that ChatGPT used 100 nvidia chips to achieve a certain task and its valuation was at 100 billion US$.
After DeepSeek's performance has been verified, it just uses 5 nvidia chips to achieve the same task. Thus, ChatGPT is revaluated to 5 billion US$.
Furthermore, if everybody uses Deepseek as his tool, he only needs 5 nvidia chips to work for him instead of 100 nvidia chips. So nvidia can only sell 5 chips to each customer instead of 100 chips. So Nvidia's valuation is also recalculated to be 5% of its old value.
It explains recent stock exchange shock.
So far what I see is people are proud of their AI initiatives and will readily brag about how much it improves their productivity, even if it is just used to generate generic responses such as thank you notes. One thing to worry about with most on-line AI is that you are giving as much info as you are getting.
So far what I see is people are proud of their AI initiatives and will readily brag about how much it improves their productivity, even if it is just used to generate generic responses such as thank you notes. One thing to worry about with most on-line AI is that you are giving as much info as you are getting.