Member's Forum steppers (x4)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 627 subscribers
  • Views 2412 views
  • Users 0 members are here
  • pico
  • stepper
  • PIO
Related

steppers (x4)

Jan Cumps
Jan Cumps over 1 year ago

Can you have enough stepper motors? Maybe.

I did an investment. I had one driver IC and a good motor. I added 4 somewhat heavier motors, and 4 Allegro A4988 drivers.

image

(for my own documentation)

  • Motor Type: Bipolar Stepper
  • Step Angle: 1.8 deg.
  • Holding Torque: 40N.cm (56oz.in)
  • Rated Current/phase: 1.7A
  • Phase Resistance: 1.5Ohm±10%
  • Insulation Resistance: 100MΩ¸ Min, 500VDC
  • Insulation Strength: 500VAC for one minute
  • Physical Specification:
  • Frame Size: 42 x 42mm (1.7 inch x 1.7 inch)
  • Body Length: 40mm
  • Shaft Diameter: 5mm
  • Number of Wire Leads: 4
  • Wire Length: 400mm
  • Weight: 280g
  • Temperature rise: 80deg Max(rated current, 2 phase on)


Rood B+
Groen A-
Zwart A+
Blauw B- 

image

One more strange stepper is on its way from China:
image, 

Goal is to control them with a single Pico.

  • Sign in to reply
  • Cancel
  • robogary
    robogary over 1 year ago

    I look forward to see what you create with the steppers. I got a couple, they are too heavy for my small robots and projects. 

    I really wanted to try out the linear gear with stepper to see if the linear speed can be useful without jamming. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 1 year ago

    This reminded me of a rather heavy box of motors I have. There's a healthy mix of servos, dc motors with reduction gears, and steppers (most of them salvaged from old equipment). I've been telling myself that I'll find a use for them for like 10 years, and I intend to keep telling myself that for several years more :D

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 1 year ago

    I look forward to seeing what you make with them.

    I have a bunch of stepper motors I salvaged from old printers and CD/DVD drives.

    Maybe I will get ambitious and make a project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to anniel747

    description says it's for (or from) an engraver

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<