Member's Forum Question of the Month: What’s the most frustrating part of working with modern micro-controllers?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 626 subscribers
  • Views 3438 views
  • Users 0 members are here
  • poll
  • QOM
  • question of the month
Related

Question of the Month: What’s the most frustrating part of working with modern micro-controllers?

cstanton
cstanton over 1 year ago

Micro-controllers are at the core of most embedded systems, but working with them isn’t always smooth. From confusing datasheets to fragmented tool-chains, even experienced engineers can hit roadblocks. This month, we want to know:

Bonus question:

What micro-controllers are you currently using? (and why that one?)

  • Sign in to reply
  • Cancel
  • m.ahtisham.khan
    m.ahtisham.khan over 1 year ago

    Using multiple STM32 series, ESP32-S3/C3, but when targeting wearable devices or battery-operated devices or BLE applications, nRF52840 or nRF52832 are best in terms of current consumption. For NB-IoT applications, nRF9160 is also a great option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • FreeBird
    FreeBird over 1 year ago in reply to robogary

    I think when I took that class it was Threetran :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 1 year ago in reply to rsc

    I have the same MO.  It got particularly bad when there were part shortages.  I bought a lot of stuff whenever it became available even when I didn't need it.

    That's one reason that I like the Seeed Xiao.  I have 9 different MCU types in the same footprint so that it is easier to try different MCUs for the same project.

    I also have all the RPi and Pico variants.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 1 year ago

    My SOP is to have at least one of everything..... just in case......I think the RPis are self-replicating in the cabinet....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 1 year ago in reply to DAB

    I still have a few 572B's and 811A's in the basement.......

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 1 year ago in reply to Robert Peter Oakes

    No Peter, you are still a youngster.

    I am old, I started with vacuum tubes.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 1 year ago

    Reading all of this makes me think of a few things

    I've been programming and coding since 1976, starting with PDP8 and 11, 8080 in the form of an S100 bus system configured for industrial control and even a little cobol on the company mainframe. since then probably coded in dozens of languages over the years, mainly changing because the new job had X as the standard, I think if you know how to design a good program it becomes easier to code it for a specific MCU/CPU

    Even after over 50 years I still drop to C++ as my goto with C# when targeting MS platforms.

    I like the abstraction from hardware to user code of things like the arduino IDE, its hard to say the board is an arduino anymore but I really like the code abstraction, 99% or more of applications dont need the speed of assembly or other direct platform written code and were you need a bit more power you can switch out the hardware with little change to you actual code, were you do then drop to C++ or something.

    on the STM development environment I love the configurator/mapper that allows internal function blocks to be configured and or mapped to external pins in some cases almost any pin, that's awesome and can aid in pcb layout tremendously i think.

    Distributed computing / environment is the way to go for all but the simpler systems, even now with 3D printing or other CNC/motion control type solutions there are apps like Klipper that abstract the G Code interpretation and hans of just motion control to one or more MCU's for the various parts of in my canse the 3D printer.

    I am building 2 right now, a Voron Trident and a Voron V2 R2.4, both have a PI or equivalent for the master controller and then in my case a RPI2040 based head controller for hotend temp, filament flow, cooling fans and the like, then another RPI2040 running the A/B motors for the core XY motion platform, then an ST32xxx based board running the heated bed, 3 or 4 Z motors , system cooling and various other things. The PI is also providing web interface and local display / controls.

    That's all for just a 3D printer but it keeps everything simple, the environment is abstracted but highly optimized for near real time control of those motors (Gotta make sure those circles are actually round :) ) and it supports loads of different MCU's and hardware interfaces.

    I could go on but I digress, I will be creating posts for the 3D printer builds in detail soon but thats were im at for now with coding and building.

    Oh... yes im old too Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Chip
    Chip over 1 year ago

    Dyslexic .  I got a copy and paste everything to enough app get read to me . Someone type the question why not just put the voice over the top as well  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mhenman
    mhenman over 1 year ago

    I still use a lot of PIC16f series MCUs, mostly because I bought a ton of them years ago and have been slowly dwindling my stock.  My new goto MCU when I need more power is definitely the ESP32S3.  Amazing bang for the buck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Instructorman
    Instructorman over 1 year ago

    STM32F732.  Wanted to learn more about ARM processors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>