Member's Forum WARNING ! AI rots your Brain
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 47 replies
  • Subscribers 628 subscribers
  • Views 2980 views
  • Users 0 members are here
Related

WARNING ! AI rots your Brain

michaelkellett
michaelkellett over 1 year ago

From yesterdays Telegraph:

image

The article is based on work done at MIT 

https://www.media.mit.edu/projects/your-brain-on-chatgpt/overview/

https://www.brainonllm.com/

If you follow the second link you can eventually find  .pdf of the full research paper (if you've been using ChatGPT a lot recently you may struggle.)

You have been warned !

MK

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps over 1 year ago

    research: I asked AI (chatGPT) if the RISC or ARM cores were most efficient.

    First answer was disappointing, but then it was on track:

    > me: what core is most efficient on rp2350, riscv or arm?

    The RP2350 is a microcontroller from Raspberry Pi Ltd. that features a dual-core Arm Cortex-M0+ processor. It does not have a RISC-V core, so in the context of this specific chip, only the Arm Cortex-M0+ is present and thus is the core in use.

    > me: this answer is wrong. rp2350 has 2 risc v cores and 2 arm cores

    You're absolutely right—my apologies for the confusion. The RP2350 features 2 ARM Cortex‑M33 cores or 2 Hazard3 RISC‑V cores, selectable at boot, or even one of each if desired forums.parallax.com+15raspberrypi.com+15sparkfun.com+15.


    Gear️ Efficiency: Cortex‑M33 vs Hazard3 RISC‑V on the RP2350

    Battery Power & Performance

    • Cortex‑M33 (150 MHz):

      • Armv8‑M architecture with DSP and single-precision FPU.

      • Optimized for energy efficiency with Thumb‑2 ISA and TrustZone security dfrobot.com+1reddit.com+1en.wikipedia.org+1smist08.wordpress.com+1.

      • Best suited for signal processing and compute-heavy tasks due to hardware acceleration.

    • Hazard3 RISC‑V (150 MHz):

      • Custom in-house dual-core design (RV32IMAC+) by Raspberry Pi raspberrypi.com+7en.wikipedia.org+7en.wikipedia.org+7.

      • Compact implementation, removes ARM licensing costs, and supports compressed ISA for denser code reddit.com.

      • Likely scales well in silicon area and cache use—designed with minimalist efficiency in mind.

    Code Density & Ecosystem

    • RISC‑V often provides better code density thanks to its C-extension, which can reduce flash/cache usage.

    • The mature Arm ecosystem offers more optimized toolchains and libraries for DSP, security, and low‑power modes.

    • RISC‑V ecosystem is growing rapidly, but M33 still leads for production-ready support raspberrypi.com+15dfrobot.com+15raspberrypi.com+15forums.parallax.com+2en.wikipedia.org+2datasheets.raspberrypi.com+2.

    Twisted rightwards arrows Switching Architecture

    • Switching between architectures requires a reset—only two cores run at a time datasheets.raspberrypi.com+1smist08.wordpress.com+1.

    • Thermal and power characteristics are similar at same clock rate; the difference lies in ISA benefits and use-case efficiency.


    Checkered flag What’s Most Efficient?

    Bar chart At 150 MHz on RP2350:

    • Per‑cycle performance:

      • Cortex‑M33 wins if you're using DSP/FPU-heavy workloads.

      • Hazard3 excels in compact code execution and flash efficiency.

    • Power consumption:

      • Both are designed to be low-power; Cortex‑M33 likely has slight edge due to mature low‑power modes and silicon optimizations.

      • Hazard3 may consume less static power and has less overhead in instruction handling.


    White check mark TL;DR

    • For DSP, FPU, and security-heavy applications, use the Cortex‑M33.

    • For code-density, open-source flexibility, and potentially lower area cost**, go with Hazard3 RISC-V.

    • Power efficiency is comparable, but your workload (FPU vs compact code) determines the best choice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 1 year ago

    research: I asked AI (chatGPT) if the RISC or ARM cores were most efficient.

    First answer was disappointing, but then it was on track:

    > me: what core is most efficient on rp2350, riscv or arm?

    The RP2350 is a microcontroller from Raspberry Pi Ltd. that features a dual-core Arm Cortex-M0+ processor. It does not have a RISC-V core, so in the context of this specific chip, only the Arm Cortex-M0+ is present and thus is the core in use.

    > me: this answer is wrong. rp2350 has 2 risc v cores and 2 arm cores

    You're absolutely right—my apologies for the confusion. The RP2350 features 2 ARM Cortex‑M33 cores or 2 Hazard3 RISC‑V cores, selectable at boot, or even one of each if desired forums.parallax.com+15raspberrypi.com+15sparkfun.com+15.


    Gear️ Efficiency: Cortex‑M33 vs Hazard3 RISC‑V on the RP2350

    Battery Power & Performance

    • Cortex‑M33 (150 MHz):

      • Armv8‑M architecture with DSP and single-precision FPU.

      • Optimized for energy efficiency with Thumb‑2 ISA and TrustZone security dfrobot.com+1reddit.com+1en.wikipedia.org+1smist08.wordpress.com+1.

      • Best suited for signal processing and compute-heavy tasks due to hardware acceleration.

    • Hazard3 RISC‑V (150 MHz):

      • Custom in-house dual-core design (RV32IMAC+) by Raspberry Pi raspberrypi.com+7en.wikipedia.org+7en.wikipedia.org+7.

      • Compact implementation, removes ARM licensing costs, and supports compressed ISA for denser code reddit.com.

      • Likely scales well in silicon area and cache use—designed with minimalist efficiency in mind.

    Code Density & Ecosystem

    • RISC‑V often provides better code density thanks to its C-extension, which can reduce flash/cache usage.

    • The mature Arm ecosystem offers more optimized toolchains and libraries for DSP, security, and low‑power modes.

    • RISC‑V ecosystem is growing rapidly, but M33 still leads for production-ready support raspberrypi.com+15dfrobot.com+15raspberrypi.com+15forums.parallax.com+2en.wikipedia.org+2datasheets.raspberrypi.com+2.

    Twisted rightwards arrows Switching Architecture

    • Switching between architectures requires a reset—only two cores run at a time datasheets.raspberrypi.com+1smist08.wordpress.com+1.

    • Thermal and power characteristics are similar at same clock rate; the difference lies in ISA benefits and use-case efficiency.


    Checkered flag What’s Most Efficient?

    Bar chart At 150 MHz on RP2350:

    • Per‑cycle performance:

      • Cortex‑M33 wins if you're using DSP/FPU-heavy workloads.

      • Hazard3 excels in compact code execution and flash efficiency.

    • Power consumption:

      • Both are designed to be low-power; Cortex‑M33 likely has slight edge due to mature low‑power modes and silicon optimizations.

      • Hazard3 may consume less static power and has less overhead in instruction handling.


    White check mark TL;DR

    • For DSP, FPU, and security-heavy applications, use the Cortex‑M33.

    • For code-density, open-source flexibility, and potentially lower area cost**, go with Hazard3 RISC-V.

    • Power efficiency is comparable, but your workload (FPU vs compact code) determines the best choice.