Member's Forum Question of the Month: What design feature do you think is overused, something added out of habit rather than real need?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 592 subscribers
  • Views 1600 views
  • Users 0 members are here
  • question of the month
  • overused design
Related

Question of the Month: What design feature do you think is overused, something added out of habit rather than real need?

cstanton
cstanton 6 months ago

What's a design element or feature you think is overused, something people include out of habit rather than necessary?

When planning a project, it's easy to add unnecessary features in the design phase. These are the "just in case" or "that's how it's always done," but sometimes, those extra elements can add cost, complexity, or waste without really improving the project.

Bonus question: What design feature do you believe is underused?

  • Sign in to reply
  • Cancel

Top Replies

  • rsc
    rsc 6 months ago +6
    Overused - Software that can't be used without an internet connection. On several field experiments, we were out in the ocean with no internet and several instruments could not be used. Underused …
  • dougw
    dougw 6 months ago +5
    How about subscription based "products" where you never own anything, just pay every month regardless of whether you use it.
  • genebren
    genebren 6 months ago +3
    Complexity - I tend to like to keep it simple. I have always found that small microcontrollers, with clean and simple tools set are easier to use and provide a quicker turnaround time for designs. I am…
Parents
  • dougw
    dougw 6 months ago

    Underused is great question. One thing I find annoying is the practise of minimizing the number of buttons, which ends up making the user interface slow, complex and non-intuitive. Think household thermostats. Does anybody remember how to program a VCR? Buttons can also be overused - like up/down buttons when a volume knob or slider is faster and more intuitive. Remember when you could just rotate a dial to the temperature you wanted.

    Remember when microcontrollers and SBCs came with a "monitor"  - a supervisory program that would allow direct control of all I/O or examining/altering memory. I miss that functionality. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller 6 months ago in reply to dougw
    dougw said:
    Remember when microcontrollers and SBCs came with a "monitor"  - a supervisory program that would allow direct control of all I/O or examining/altering memory. I miss that functionality. 

    This. This is why computers should still have front panels. Plus you get a free light show.

    Why yes, I do have a PiDP-10. obsolescence.wixsite.com/.../pidp10

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw 6 months ago in reply to bradfordmiller

    While at university, I was so hungry to learn more about computers, I took a night course at a local community college to see what they offered. It turned out they were still using PDP8 (at Uni we were using PDP11) and our first assignment was entering a program using the front panel toggle switches. Later the course allowed the use of paper tape to enter programs, for those that remember that technology.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren 6 months ago in reply to dougw

    I did a lot of work with military computers (ruggedized Data General computers) during my first job.  I could entry the 20+ instructions for the paper tape bootloader, on the front panel from memory.  I wrote a bunch of diagnostics, that when running would read the address switches, then display the contents of the address on to the data lights as a sort of "PEAK" to allow be to monitor attached hardware for trouble shooting. Fun times!  I have been so tempted to build a clone of these early computers using a simple microprocessor as a retro display piece.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller 6 months ago in reply to genebren

    Many early computers can be simulated using simh. The work Oscar has done with obsolescence guaranteed has created ⅔ models for front panels for various DEC machines (8, 11, 10, 1 .. so far) that uses simh running on an RPi. He's also rumored to be working on a TX-2...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bradfordmiller
    bradfordmiller 6 months ago in reply to genebren

    Many early computers can be simulated using simh. The work Oscar has done with obsolescence guaranteed has created ⅔ models for front panels for various DEC machines (8, 11, 10, 1 .. so far) that uses simh running on an RPi. He's also rumored to be working on a TX-2...