Member's Forum The Ultimate Project Kit?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 628 subscribers
  • Views 2527 views
  • Users 0 members are here
  • dougw
  • ideal project kit
Related

The Ultimate Project Kit?

dougw
dougw 11 months ago

The question is what constitutes an ideal project kit?

Of course it is going to be impossible to come up with a universal set of building blocks that covers every application, but given a fairly generic set of basic building blocks, what would be the most common solution that you would propose - to fit more applications than other solutions?

Assume a generic project would include a microcontroller, a sensor, an actuator, a user interface, and a power supply.

What else? Would you include signal conditioning circuits or amplifiers? Would you include audio components? Would you include LEDs?

To get the ball rolling, I would suggest 2 scenarios - a high end kit and a lower end kit.

For the high end kit I would go with an Arduino Giga with its touch LCD, a ToF Laser Ranging Sensor, a servo motor, and a USB C power module. The Giga could use a small powered speaker as a nice option.

For the lower kit I would go with an Arduino Nano R4 and a 1" OLED display instead of the Giga but keep the ToF sensor, servo and USB C power.

I expect others will prefer a Raspberry Pi to a Giga, but we will find out in the comments.

Leave a comment to elaborate on your thinking.

  • Sign in to reply
  • Cancel
Parents
  • dang74
    dang74 11 months ago

    The industry has moved away from this direction but I'd like a dev board that featured a modern ARM micro that brought out a substantial parallel bus to a header.  Then I'd like an FPGA daughter card with a mating header.  The idea would be to decode the bus in the FPGA and create a custom peripheral.  What can I say, PC104 left an impression on me.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • bradfordmiller
    bradfordmiller 11 months ago in reply to dang74

    I'd skip the micro and just use some kind of Zynq. And since it's the "ultimate" project kit, we'd want to be able to easily add 100G ethernet, Wifi 9, PB of Infineon memory, ... at least an FPGA gives us some hope of evolving for future interfaces. Plus we'd want to be able to hook multiple mainboards together into a (Beowulf :-) cluster.

    Really the problem with anything "ultimate" is either it can evolve into something still useful in a hundred years, or it will be dated a couple years after it's set (so not really "ultimate", or even "penultimate").

    Anyway on a more serious note, if it's not reconfigurable, (i.e. like an FPGA) then I think it will miss the mark of really broad applicability.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bradfordmiller
    bradfordmiller 11 months ago in reply to dang74

    I'd skip the micro and just use some kind of Zynq. And since it's the "ultimate" project kit, we'd want to be able to easily add 100G ethernet, Wifi 9, PB of Infineon memory, ... at least an FPGA gives us some hope of evolving for future interfaces. Plus we'd want to be able to hook multiple mainboards together into a (Beowulf :-) cluster.

    Really the problem with anything "ultimate" is either it can evolve into something still useful in a hundred years, or it will be dated a couple years after it's set (so not really "ultimate", or even "penultimate").

    Anyway on a more serious note, if it's not reconfigurable, (i.e. like an FPGA) then I think it will miss the mark of really broad applicability.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dang74
    dang74 11 months ago in reply to michaelkellett

    I like the way the varient you designed sounds.  ARM micro with Lattice FPGA in QFN package is just what the doctor ordered... and OLED is gravy.  My kind of kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett 11 months ago in reply to dang74

    This little display board is about as near as I get to a universal board. It is powered by a GigaDevices ARM processor and has serial ports for control.

    I've used it in a few projects, and it's going to be used in some more. The little 128x64 Oled displays are nice.

    image

    image

    I recently did a re-spin of it for a customer with an ST ARM processor, a small Lattice FPGA and differential line drivers and receivers for the FPGA to talk to position encoders and work its magic on them.This is nicer package and has USB C for serial comms and/or power as well as logic level UART.

    image

    image

    The Lattice FPGA is quite nice to use and reasonable to solder in this 48 pin QFN package - they get much less nice if you need more pins because Lattice only do them in very fine pitch BGA. I like that Altera still offer a lot of their parts in TQFP packages - I wish Xilinx would. (I'm getting cheesed off with calling them Intel and AMD (and of course Altera is back to being Altera now)).

    MK

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 11 months ago in reply to bradfordmiller

    I contemplated having something with an embedded hard processor in the FPGA like a ZYNQ, but ideal or not, I wanted to keep cost and complexity down.  For instance the FPGA board would be one of those QFP-144 types that sell for less than $25.  A couple of years ago I designed an FPGA daughter board for Cyclone IVE and Cyclone 10 devices.  I did not design any mother boards though.image

    • Cancel
    • Vote Up +3 Vote Down