Member's Forum What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 71 replies
  • Subscribers 593 subscribers
  • Views 11700 views
  • Users 0 members are here
  • element14 community
  • win
  • element14 members
  • aske14
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition

E14Alice
E14Alice 1 month ago

A new month means a new AskE14!

Engineers, makers, and problem‑solvers are always finding smarter ways to work. From optimising workflows to automating repetitive tasks, small habits can add up to serious time savings.

This month, AskE14 is all about sharing the habits that help you work more efficiently, whether you’re designing, prototyping, debugging, documenting, or managing projects.

Time for the question:

What’s the most time-saving habit you’ve picked up? 

Time is a valuable resource in engineering. A simple habit — like better version control, smarter test setups, or clearer documentation. This can save hours down the line.

imageimage

Competition Details

You'll have to be a member of the element14 Community to join in and take part in this “Join, Share & Win” challenge. It's simple, all you have to do is:


1. You need to make sure you are  Register  or Login
2. Then answer the following question by adding a reply or commenting!

What’s the most time-saving habit you’ve picked up? 

This month, we are giving away:

The Community team will then select the best 3 answers to win the UNO R4 Minima! 

image

Closing date: 1st March 

Winners announced: 10th March 

UNO R4 Minima  

Terms and Conditions 

imagePDF

The winners! 

dang74 

wolfgangfriedrich 

skruglewicz 

E14Alice will be reaching out to you soon to confirm contact details

  • Cancel

Top Replies

  • dang74
    dang74 1 month ago +5
    For hobby projects I've been pasting code into ChatGPT so that it can fulfill the role of a peer review. It has caught many dumb mistakes that would have otherwise gone unnoticed until the debug stage…
  • Arnovsharma
    Arnovsharma 1 month ago +5
    The habit that has been most valuable to me is to document my work as I do it, rather than later. This includes: Maintaining a simple project log (even in a notebook or text file). Recording why…
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago +5
    Simulate critical parts of the design. If the simulation works, chances are that you saved one iteration of design and the likelihood of the 1st prototype working increased by a lot. If the simulation…
Parents
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago

    Simulate critical parts of the design. If the simulation works, chances are that you saved one iteration of design and the likelihood of the 1st prototype working increased by a lot. If the simulation fails, the hardware will fail for sure. 

    • Cancel
    • Vote Up +5 Vote Down
    • Cancel
Reply
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago

    Simulate critical parts of the design. If the simulation works, chances are that you saved one iteration of design and the likelihood of the 1st prototype working increased by a lot. If the simulation fails, the hardware will fail for sure. 

    • Cancel
    • Vote Up +5 Vote Down
    • Cancel
Children
  • Aniket_kumar_raj
    Aniket_kumar_raj 1 month ago in reply to wolfgangfriedrich

    Woh, that's what I need to, what's the simulation software is called,I used tinkercad but that for limited

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago in reply to Aniket_kumar_raj

    LTspice for discrete circuits and ModelSim for VHDL design. 
    And then there is QSpice which claims to be able to simulate digital (C, VHDL) and discrete components in the same design, but I did not have time to try it out properly.

    And for simple stuff there is always a handheld calculator and Brain1.0

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • battlecoder
    battlecoder 1 month ago in reply to wolfgangfriedrich

    I've been doing some simulations in LTSpice lately, and it's made so much easier and faster to test stuff out. They also help me figure out if something works or not before even hitting the breadboard so I agree!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • michaelkellett
    michaelkellett 1 month ago in reply to wolfgangfriedrich

    LT Spice is one of very few things which is both good and free. It does rather push you towards the Analog Devices part for any given job (assuming they make one) because it only includes ready to use models for their chips (although you can use spice models from other manufacturers with a little bit of effort (although they don't always work)).

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • BigG
    BigG 1 month ago in reply to wolfgangfriedrich

    I certainly need to do this more often. I've had a case where hardware did fail and on close inspection of the design had identified an issue, but could not quite explain the why. Other engineers had other ideas. It was most satisfying when the LTspice simulation was completed, and it was able to not only mimic the failure but was also able to show why the attempted fixes did not work. It then proved the hunch.

    These days you can simulate directly via KiCAD. So no excuses.