Member's Forum What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 71 replies
  • Subscribers 593 subscribers
  • Views 11749 views
  • Users 0 members are here
  • element14 community
  • win
  • element14 members
  • aske14
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition

E14Alice
E14Alice 1 month ago

A new month means a new AskE14!

Engineers, makers, and problem‑solvers are always finding smarter ways to work. From optimising workflows to automating repetitive tasks, small habits can add up to serious time savings.

This month, AskE14 is all about sharing the habits that help you work more efficiently, whether you’re designing, prototyping, debugging, documenting, or managing projects.

Time for the question:

What’s the most time-saving habit you’ve picked up? 

Time is a valuable resource in engineering. A simple habit — like better version control, smarter test setups, or clearer documentation. This can save hours down the line.

imageimage

Competition Details

You'll have to be a member of the element14 Community to join in and take part in this “Join, Share & Win” challenge. It's simple, all you have to do is:


1. You need to make sure you are  Register  or Login
2. Then answer the following question by adding a reply or commenting!

What’s the most time-saving habit you’ve picked up? 

This month, we are giving away:

The Community team will then select the best 3 answers to win the UNO R4 Minima! 

image

Closing date: 1st March 

Winners announced: 10th March 

UNO R4 Minima  

Terms and Conditions 

imagePDF

The winners! 

dang74 

wolfgangfriedrich 

skruglewicz 

E14Alice will be reaching out to you soon to confirm contact details

  • Cancel

Top Replies

  • dang74
    dang74 1 month ago +5
    For hobby projects I've been pasting code into ChatGPT so that it can fulfill the role of a peer review. It has caught many dumb mistakes that would have otherwise gone unnoticed until the debug stage…
  • Arnovsharma
    Arnovsharma 1 month ago +5
    The habit that has been most valuable to me is to document my work as I do it, rather than later. This includes: Maintaining a simple project log (even in a notebook or text file). Recording why…
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago +5
    Simulate critical parts of the design. If the simulation works, chances are that you saved one iteration of design and the likelihood of the 1st prototype working increased by a lot. If the simulation…
Parents
  • bradfordmiller
    bradfordmiller 1 month ago

    When writing code I generally work bottom up and, I also write the test cases for that code (based on the spec), which can be commented out (or in a separate file not normally loaded). Then I can test each module separately which saves a lot of time during integration (higher level testing) as the lower level parts are known to meet their specification. Additionally some of these tests (e.g., type validation of arguments) can be added directly into the code but suppressed for higher optimization levels (i.e. for delivery).

    Design by contract languages may help with this as well, though I'm not currently using one. I suppose this would be the moral equivalent of using SystemVerilog for testbenches, but something that can be carried around in code that is actually being executed on the target rather than only in simulation.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • bradfordmiller
    bradfordmiller 1 month ago

    When writing code I generally work bottom up and, I also write the test cases for that code (based on the spec), which can be commented out (or in a separate file not normally loaded). Then I can test each module separately which saves a lot of time during integration (higher level testing) as the lower level parts are known to meet their specification. Additionally some of these tests (e.g., type validation of arguments) can be added directly into the code but suppressed for higher optimization levels (i.e. for delivery).

    Design by contract languages may help with this as well, though I'm not currently using one. I suppose this would be the moral equivalent of using SystemVerilog for testbenches, but something that can be carried around in code that is actually being executed on the target rather than only in simulation.