Member's Forum The Definitive Collection of V.90/V.92 Dial-Up Modem Sounds
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 631 subscribers
  • Views 4367 views
  • Users 0 members are here
  • audio
  • vintage
  • pots
  • modem
  • history
  • telephony
  • blog
  • connectivity
Related

The Definitive Collection of V.90/V.92 Dial-Up Modem Sounds

Gough Lui
Gough Lui over 10 years ago

Hi fellow Vintage Tech subscribers.

 

First post in this area, and I thought I'd make it about the voice-band modem technology which is fast fading away. The V.90 and V.92 standard are special, in that they exploited the fact that one side of the connection can be purely digital, and thus suffers less distortion from analog to digital conversion, and vice versa. As a result, V.90/92 connections can only happen with digital modem terminating gear, making them unlikely to be achieved once the existing modem banks operated by commercial ISPs are closed down.

 

The V.90 standard was a compromise standard that was incompatible with the warring x2 and K56flex standards of the early 56k days. The V.90 standard introduced a new signal, known as a Digital Impairment Learning (DIL), which is defined by the analog modem in a data segment known as Ja, and sent back from the digital modem so that the analog modem can learn of the impairments on the line (e.g. digital pads, robbed bit signalling). The way this is defined led to different chipsets having a different DIL due to their differing software algorithms.

 

In order to capture this, I bolstered my collection of modems, got my VoIP gear configured carefully to best pass data and made many test-calls to commercial ISP lines to reconstruct the calls and produce the highest quality samples which cover virtually all chipsets, with the exception of Topic/ICPlus.

 

You will find the post at:

http://goughlui.com/2016/05/03/project-the-definitive-collection-of-v-90v-92-modem-sounds/

 

I hope you enjoy it - feel free to browse the related modem collection, and project FAX area for more voice-band modem goodness.

 

- Gough

  • Sign in to reply
  • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Gough Lui

    Most faster modems are pretty smart and will look for an "AT" to set its internal baud rate

    The serial port was a dumb port, and the call was initiated from external.

    So yes we needed to lock the DTE rate regardless of the DCE (modem to modem) speed.

     

    One of the customers always used a MultiTech modem with all the bells and whistles, but never used the Dial back feature.

     

    All in all we never really had many issues with the modems, once they were setup.

    Eventually we made a script under ProComm to do all the settings which eleminated the human error and saved a few brain cells.

    (I'll get back to you later if the brain cell saving worked)

     

    This modem thing is a whole life that the newer generation will never get to experience.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to mcb1

    Autobaud not reliable enough? or a lack of flow control with a slow CPU?

     

    Most faster modems are pretty smart and will look for an "AT" to set its internal baud rate. As far as I've seen, I've never had it miss, at least with the standard IBM rates (300, 1200, 2400, 4800, 9600, 19200, 38400, 57600, 115200, 230400) with most chipsets. Some chipsets are even smart enough to only negotiate DCE to DCE rates below the DTE to DCE rate, so if you open the port at 2400bps and issue an ATD... command, it will "naturally" limit the modulation to prevent overflow at the modem.

     

    Of course, if you know your port is only going at one rate, and absolute mission-critical reliability was the aim, then I suppose there's nothing wrong with locking the rates. It means a little extra work image. I know some guys that use the dial-up modem still today as a back-up emergency telemetry and telecommand system and have it set up to do dial-back and other fancy tricks which consumer modem firmware doesn't have. They chose some very nice and shiny MultiTech modems with internal intelligence to do it, whereas some of the other vendors (e.g. Netcomm Wireless) have all-integrated industrial modems with an access control system inbuilt.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to clem57

    You may have a grudge against the vendors and their semi-arbitrary choices of AT commands for the same "features", but this came about because the company that first bought in the smart-modem (Hayes) essentially lost market leadership and control of the command set, and others were probably afraid of litigation due to copying the other vendor's commands (e.g. the +++ escape sequence resulted in the semi-compatible +++AT "time independent" escape sequence, aka TIES). The later modems, not hamstrung by the expense of ROM/EEPROM/Flash memory, started replying nicely if you enquired it about its value (AT+MS?) and also responded as to the values it would accept (AT+MS=?), so you could poke around even without the AT command reference.

     

    at+ms=?

    +MS: (0,1,2,3,9,10,11,56, 64,69),(0,1),(300-33600),(300-56000),(0,1),(0,1)

    OK

     

    On the whole, at least dealing with later modems, the important commands are easier to remember because they became less bit-mapped S-register values, and more "actual" values with onboard help. Modulation-select commands were common to "help" stabilize modems by limiting their connect rate, and since most modems were Rockwell/Conexant based, the first port of call was AT+MS, whereas the Lucent/Agere had AT-V90 and some others had no options at all.

     

    Modems also had nice diagnostic output, at least some of them, but again, different chipsets had different tendencies. USRobotics/Texas Instruments based modems were ATI6 and ATI11 with ATY11 line frequency-attenuation readout capability that no other modems had, whereas Lucent/Agere stuck with ATI11, Broadcom was ATI6 & ATI11. Oddball Rockwell/Conexant had older modems responding to AT&V1 (as did Motorola), and later modems with AT#UG. Ambient/Intel chose ATI20.

     

    e.g. ATI6, ATI11 from TI chipset

    ati6

     

    U.S. Robotics 56K Professional Message  Link Diagnostics...

     

    Chars sent                    3      Chars Received               82

    Chars lost                    0

    Octets sent                   3      Octets Received              82

    Blocks sent                   3      Blocks Received               4

    Blocks resent                 0

     

    Retrains Requested            0      Retrains Granted              0

    Line Reversals                0      Blers                         1

    Link Timeouts                 0      Link Naks                     0

     

    Data Compression       V42BIS 512/16

    Equalization           Long

    Fallback               Enabled

    Protocol               LAPM

    Speed                  42666/28800

    V.90 Peak Speed        42666

    Current Call           00:00:11

     

    Online

     

    OK

    ati11

     

    U.S. Robotics 56K Professional Message  Link Diagnostics...

     

     

    Modulation                  V.90

    Carrier Freq     (Hz)       None/1920

    Symbol Rate                 8000/3200

    Trellis Code                None/64S-4D

    Nonlinear Encoding          None/ON

    Precoding                   None/ON

    Shaping                     ON/ON

    Preemphasis      (-dB)      0/4

    Recv/Xmit Level  (-dBm)     8/16

    Near Echo Loss   (dB)       2

    Far Echo Loss    (dB)       0

    Carrier Offset   (Hz)       NONE

    Round Trip Delay (msec)     585

    Timing Offset    (ppm)      18244

    SNR              (dB)       41.9

    Speed Shifts Up/Down        0/0

    Status :                    ua,5,12N,12.2,-8,0N,0,41.2,23.7

    OK

    e.g. ATI11 from LT/Agere

     

    ati11

     

     

        Description                         Status

        ---------------                     ------------

        Last Connection                     NA             

        Initial Transmit Carrier Rate       NA             

        Initial Receive  Carrier Rate       NA             

        Final   Transmit Carrier Rate       NA             

        Final   Receive  Carrier Rate       NA             

        Protocol Negotiation Result         NA             

        Data Compression Result             NA             

        Estimated Noise Level               NA             

        Receive  Signal Power Level  (-dBm) NA             

        Transmit Signal Power Level  (-dBm) NA             

        Round Trip Delay             (msec) NA             

    Press any key to continue; ESC to quit.

     

        Description                         Status

        ---------------                     ------------

        Near Echo Level              (-dBm) NA             

        Far  Echo Level              (-dBm) NA             

        Transmit Frame Count                0              

        Transmit Frame Error Count          0              

        Receive  Frame Count                0              

        Receive  Frame Error Count          0              

        Retrain by Local  Modem             0              

        Retrain by Remote Modem             0              

        Call Termination Cause              0              

        Robbed-Bit Signaling                NA             

        Digital Loss                   (dB) NA             

        Remote Server ID                    NA             

     

    OK

    e.g. AT#UG from Conexant HSFi

    at#ug

    <VERSION=10>

    <CALL SETUP RESULT=Detected Data Answer Tone>

    <MULTIMEDIA MODE=Data Only>

    <DTE-DCE MODE=Async data>

    <V.8 CM octet string="">

    <V.8 JM octet string="C16513948">

    <RX SIG POWER DB=16, TX SIG POWER DB=18, S/N RATIO DB=40>

    <NORMALIZED MEAN SQUARED ERROR=48>

    <NEAR ECHO LOSS=6>

    <FAR ECHO LOSS=200>

    <FAR ECHO DELAY=177>

    <ROUND TRIP DELAY=177>

    <V.34 INFO bit map =0>

    <TX MOD=V.90, TX SYMBOL RATE=3200, TX CARRIER FREQ=1920>

    <RX MOD=V.90, RX SYMBOL RATE=8000, RX CARRIER FREQ=0>

    <TX FIRST DATA RATE=28800, RX FIRST DATA RATE=46667>

    <CARRIER LOSS=0, RATE RENEG=0>

    <RETRAINS REQ=0, RETRAINS DET=0>

    <TX FINAL RATE=28800, RX FINAL RATE=46667>

    <PROTOCOL NEGOTIATION=LAPM>

    <EC FRAME SIZE=80>

    <EC LINK TIMEOUTS=0>

    <EC LINK NAKS=0>

    <COMPRESSION NEGOTIATION=V42BIS>

    <COMPRESSION DICTIONARY SIZE=800>

    <TX FLOW CONTROL=2>

    <RX FLOW CONTROL=2>

    <TX CHARS SENT FROM DTE=9>

    <RX CHARS SENT TO DTE=3F>

    <TX CHARS LOST=0>

    <RX CHARS LOST=0>

    <TX FRAME COUNT=8>

    <RX FRAME COUNT=4>

    <TX FRAME ERROR COUNT=3>

    <RX FRAME ERROR COUNT=0>

    <TERMINATION CAUSE=No previous call>

    <CALL WAITING EVENT COUNT=0>

    <LSD Vdd=56806200, Power Bits=362CB38>

    <V8BIS FLEX VERSION=0, V8BIS DSP VERSION=0>

    <RATE RENEG REQ=0, RATE RENEG DET=0>

    <HIGH PASS FILTER ENABLED=0>

    <ROBBED BIT PATTERN=EB>

    <DIGITAL PAD DETECTED=0, DIGITAL LOSS ESTIMATE=0>

    <Cnt1=0, Det1=0, Res1=0>

    <EQM=30, TRAINING EQM SUM=30>

    <NEGOTIATION TIME=22854>

     

    OK

     

    Believe it or not, Microsoft tried to have a hand in this diagnostic business, and tried to standardize a command to dump modem diagnostics. The command is AT#UD for "unimodem diagnostics", but the problem was (like in SMART) they never standardized anything aside from the dump format, so you end up with cryptic Key + Value pairs which you can only decode if the driver contains the strings which define what each key meant - and some modem manufacturers never got that far. Others really goofed up, and lost all the stats once the call was hung up, so that's very useful!

     

    e.g. AT#UD output from the SL2800:

     

    at#ud

    OK

    DIAG <2A4D3263 00=FF 01=F 02=F 03=F>

    DIAG <2A4D3263 04=000000000000000000000000>

    DIAG <2A4D3263 05=000000000000000000000000>

    DIAG <2A4D3263 16=FFFF 17=FF 18=ffffffff>

    DIAG <2A4D3263 20=ff 21=ff 22=ffffffff>

    DIAG <2A4D3263 23=ffffffff 24=ffffffff>

    DIAG <2A4D3263 25=ffffffff 26=ffffffff>

    DIAG <2A4D3263 27=ffffffff 30=FF 31=FF>

    DIAG <2A4D3263 32=FF 33=FF 34=FFFF>

    DIAG <2A4D3263 35=FFFF 40=FF 41=FFF>

    DIAG <2A4D3263 42=FF 43=FF 44=FF 45=FFFF>

    DIAG <2A4D3263 50=F 51=F 52=ffffffff>

    DIAG <2A4D3263 53=ffffffff 54=ffffffff>

    DIAG <2A4D3263 55=ffffffff 56=ffffffff>

    DIAG <2A4D3263 57=ffffffff 58=0 59=0>

    DIAG <2A4D3263 60=01 61=FF 128=ffffffff>

    On the whole, I very much liked AT commands for their simple in-band management and the fact that the S-registers reminded me of just how simple you can make your gear. Changing the S-registers are literally changing the numbers by which the modem code would use to perform its routines, and the resulting changes sometimes helped users get better compatibility of their modems (e.g. Apple users with an adapter cable use DTR signal differently to PC users, or whether the modem reported DCE to DCE or DTE to DCE speeds and what return codes it would supply), or even push the speeds (I got 54667bps connect just *once* in my lifetime, but even doing that for a fraction of a minute was an achievement).

     

    My biggest regret at this stage was not having the opportunity to document 3com/USR's x2 modulation. In Australia, I don't remember x2 being very popular, and the number of high quality x2 handshake recordings are nought (at least, to my knowledge). The number of x2 modem banks are probably very low as well, as only 3com answer equipment has a chance of supporting it, and no ISP readily advertises their gear nor their capabilities aside from the ITU standards. I never got a chance to carefully examine K56Flex either for that matter, or record it, but I do clearly remember K56Flex having 2k connection increments (44, 46, 48, 50, 52k being common speeds to see) whereas V.90 changed that to 1.333k so we got 44, 45.3, 46.6, 48, 49.3, 50.6, 52k, so an early way of telling if your modem was V.90 was to see whether it had 3's and 6/7's in the connect speed line (although if you connected at the common rates, you couldn't tell).

     

    Fond memories ... very fond memories. I was on dial-up a lot longer than I should have been, partly because of the house-hopping and renting, but it was mostly a reliable partner.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to mcb1

    I mainly was changing modems DIL to pick optimal exchanges since some of their choices conflicted with our Robotics X2 technology and failed to connect.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to clem57

    Yep been and played with a few of them.

    Luckily we were mainly dialling out in a relatively dumb mode, but we did need to start locking DTE rates when modems climbed out of the 2400 baud age. ....

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to mcb1

    You think that was fun, I found the various AT commands more intriguing with so many variations. I kept a few sheets of script notes around for help.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago

    Nice work.

    I had no idea the old dialup modem was so complicated.

     

    There is a generation that has no idea of what dial-up means, so it's nice that history is captured for the day they want to explore.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago

    The by gone era of 56K modems still ring in my memory. I was a second level tech fixing modems not connecting back in the mid 1990's for an ISP. image