Member's Forum Who's in the UK and has caved in and bought air conditioning?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 93 replies
  • Subscribers 626 subscribers
  • Views 2627 views
  • Users 0 members are here
  • air conditioning
  • heatwave
Related

Who's in the UK and has caved in and bought air conditioning?

stanto
stanto 3 months ago

I picked up something like this about three years ago. No regrets.

Though I can't help but feel like I'm also adding to the climate problem.

  • Sign in to reply
  • Cancel
Parents
  • dang74
    dang74 2 months ago

    I am in the process of watching Run Away on Netflix.  It is set in the UK and filmed there as well.  I am not sure what specific region though.  Anyway while the shots of the country side are beautiful and green they seem less green than I remember from previous trips I've taken to England... so a question for those in the UK... with the recent rise in temperatures during the last few summers are things less green now?  Or am I remembering things through 'emerald green' tinted glasses?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14phil
    e14phil 2 months ago in reply to dang74

    The UK is consistently Grey and overcast as a general rule. Except 5-8 weeks in the summer where our insulated miserable weather houses struggle with 30C and we all think about getting aircon.  The hard bit is our walls are solid with no space for ducting of any kind, so if you have the money some people end up with free standing units.  Still rare. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 2 months ago in reply to e14phil
    e14phil said:
    The hard bit is our walls are solid with no space for ducting of any kind

    I'm planning on ducting through an existing window vent (or two)  Slight smile

    Have just acquired a 6" duct fan that can move up to 402cfm, so hoping I can tap into some of the cooler evening air to help with night time sleeping, without going to full-on aircon at this stage.

    Although, I suspect that the solid walls / roof space act as a storage heaters to some extent.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy 1 month ago in reply to obones

    I understand the Bernoulli effect, but as Dave has mentioned there is a lot of more going on with the dynamics of airflow in a house that can cause it to be not effective.  Unfortunately, without doing quite a bit of experimentation/measurement I don't think that it will work for me.  Suffice to say, air intake with a low velocity fan with an outside to inside temperature differential and airflow to an open window in a second room works well and reversing the airflow does not.  In the intake scenario I have the fan mounted in the window and in the exhaust scenario I positioned the fan 1 m from the open window.  Unfortunately, this room does not have multiple windows so the airflow path is not straightforward and the air intake velocity at the remote window will be very low. With both windows in the same room exhaust might work better.  Pulling cold air from a second room's window through to the room you are trying to cool will work but with a lot longer time constant. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy 1 month ago in reply to obones

    I understand the Bernoulli effect, but as Dave has mentioned there is a lot of more going on with the dynamics of airflow in a house that can cause it to be not effective.  Unfortunately, without doing quite a bit of experimentation/measurement I don't think that it will work for me.  Suffice to say, air intake with a low velocity fan with an outside to inside temperature differential and airflow to an open window in a second room works well and reversing the airflow does not.  In the intake scenario I have the fan mounted in the window and in the exhaust scenario I positioned the fan 1 m from the open window.  Unfortunately, this room does not have multiple windows so the airflow path is not straightforward and the air intake velocity at the remote window will be very low. With both windows in the same room exhaust might work better.  Pulling cold air from a second room's window through to the room you are trying to cool will work but with a lot longer time constant.