I am using a TENMA 72-13210 programmable DC load to test my LDO DUT. However, whenever I connect the DC load to the DUT, the voltage at the point where the TENMA load inputs are connected drops to zero. I have observed the same behaviour with multiple DUTs.
My initial suspicion is that there could be an internal short circuit in the DC load. To investigate this, I disconnected the input supply to the TENMA and measured the resistance across its input terminals using a multimeter. The measured resistance was approximately 14.5 MΩ, indicating that there is no apparent short circuit across the terminals when the instrument is powered off.
However, I am not sure whether the input terminals could be getting shorted internally when the instrument is powered on, or whether this could be due to an instrument configuration or software-related issue.
Could anyone help me identify the possible causes and suggest how to debug this issue?