• Products and Partners
    Products and Partners
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
Member's Forum Cheap, silent electromechanical clock movement ideas
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 632 subscribers
  • Views 1692 views
  • Users 0 members are here
Related

Cheap, silent electromechanical clock movement ideas

pathfider1998
pathfider1998 over 9 years ago

This idea is for 7 segment electromechanical clock faces.

Using thick grease as a way to smooth out movement of colored cylinders, which is colored half-black, I use a set of cheap 12V mini fans to turn the cylinder one way around with periodic activation to keep the clock segment activated.

Cylinders automatically return to original position upon power loss or segment turning off.

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 9 years ago

    Neat displays.

    I'm just curious why you'd want to use fans and springs.

    If you were to use a stepper motor, you'd only need to power it to turn it.

     

    These are low cost 64:1 geared steppers that will turn LARGE loads.

    5V Stepper Motor

     

    Cheers

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pathfider1998
    pathfider1998 over 9 years ago in reply to mcb1

    The reason for this contraption is to minimize cable cluttering and size by limiting the number of wires and additional circuits each segment needs in order to activate a segment.

     

    Servo was out of question because it was too noisy (silent ones are very expensive), DC motors needed H-Bridge circuit, and stepper motors required at least 4 wires per segment.

     

    While using this contraption, you just need 2 wires per segment or 7 wires and 1 common bus wire, and activation can be handled with software without the need to flip the polarity. Plus, fans are cheap and silent to begin with, so I thought it was a fair choice.

     

    If you have any other ideas, please let me know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to pathfider1998

    For the logic control why not use some 1-Wire (OWP) parts such as the DS2408 addressable switches.

     

    1-Wire is being promoted at the moment.

    A Deep Dive on the Maxim 1-WireRegistered Bus with Panasonic Grid-EYERegistered Sensor and Arduino-Compatible Building Automation Platform

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pathfider1998
    pathfider1998 over 9 years ago in reply to COMPACT

    I forgot to add the line:

     

    "...and minimize the cost of producing each segment."

     

    Plus, each cylinders are about 20g (hollow plastic/softwood).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • pathfider1998
    pathfider1998 over 9 years ago in reply to COMPACT

    I forgot to add the line:

     

    "...and minimize the cost of producing each segment."

     

    Plus, each cylinders are about 20g (hollow plastic/softwood).