• Products and Partners
    Products and Partners
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
Member's Forum Cheap, silent electromechanical clock movement ideas
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 632 subscribers
  • Views 1690 views
  • Users 0 members are here
Related

Cheap, silent electromechanical clock movement ideas

pathfider1998
pathfider1998 over 9 years ago

This idea is for 7 segment electromechanical clock faces.

Using thick grease as a way to smooth out movement of colored cylinders, which is colored half-black, I use a set of cheap 12V mini fans to turn the cylinder one way around with periodic activation to keep the clock segment activated.

Cylinders automatically return to original position upon power loss or segment turning off.

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 9 years ago

    Neat displays.

    I'm just curious why you'd want to use fans and springs.

    If you were to use a stepper motor, you'd only need to power it to turn it.

     

    These are low cost 64:1 geared steppers that will turn LARGE loads.

    5V Stepper Motor

     

    Cheers

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pathfider1998
    pathfider1998 over 9 years ago in reply to mcb1

    And the cylinders are very light (optimized for low noise) so there's no need for powerful motors. Moreover this is intended to be used in less-than-10 production.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to pathfider1998

    the cylinders are very light (optimized for low noise) so there's no need for powerful motors

    I imagined they were.

    I just wondered if you were adding to the mechanical issues, rather than a bit of wiring.

     

    I was also wondering if the cyclinder could do a full turn so you don't need to reverse it.

    A simple motor to spin it until a hall effect switch detects you are there and stops.

     

    I can see the benefit for a power fail, but with the size and price of LiPo batteries, a reset to zero should be easy.

     

     

    I've learnt over the years that sometimes it is better to look at different techniques and look at the potential issues some time later.

    Generally mechanical items need lubrication or cleaning to remove gunk build-up.

     

    COMPACT

    Do you recall how your genuine ones were constructed.

    The angled edge where the segments meet must have caused some issues.

     

     

    Cheers

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to pathfider1998

    What I meant was using USB-to-serial connection to PC (with commands) as a way to set the time

    I think the same bit still applies.

     

    Both ends need to understand what is being sent and what to do with it.

     

    The Aduino Serial connection first looks to see if the IDE wants to download, and if not then the sketch runs.

    What you do with the serial port after that is up to the sketch.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 9 years ago in reply to pathfider1998

    What I meant was using USB-to-serial connection to PC (with commands) as a way to set the time

    I think the same bit still applies.

     

    Both ends need to understand what is being sent and what to do with it.

     

    The Aduino Serial connection first looks to see if the IDE wants to download, and if not then the sketch runs.

    What you do with the serial port after that is up to the sketch.

     

    Mark