• Products and Partners
    Products and Partners
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
Member's Forum Arduino Serial
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 632 subscribers
  • Views 2346 views
  • Users 0 members are here
  • arduino serial stuff
Related

Arduino Serial

roby1
roby1 over 9 years ago

Hi..i have a question, maybe a noob one for ppl who know. I have maked a counter each time when i press the button the counter increments with 1 and display on serial something like:

nr = 1, nr = 2, nr = 3 ...etc. What i wanna know and i have tryed over 4 days is how i diplay only once the value on a single line and each time when i count,  ""to somehow overwrite"" the existing value and displayng it like: ""nr = 1"" then on the same line 1 is replaced with 2..then with 3 and so on every time i count.  More simple, then same line remains unchanged and only the value get overrited (upgraded).

 

HERE IS THE CODE:

 

const int  buttonPin = 2;    // the pin that the pushbutton is attached to

const int ledPin = 10;       // the pin that the LED is attached to

 

 

// Variables will change:

int buttonPushCounter = 0;   // counter for the number of button presses

int buttonState = 0;         // current state of the button

int lastButtonState = 0;     // previous state of the button

 

 

void setup()

{

  pinMode(buttonPin, INPUT);

  pinMode(ledPin, OUTPUT);

  Serial.begin(9600);

}

 

 

 

 

void loop()

{

  buttonState = digitalRead(buttonPin);

 

 

  if (buttonState != lastButtonState)

  {

    if (buttonState == HIGH)

    {

      buttonPushCounter++;

      Serial.println("on");

      Serial.print("number of button pushes: ");

      Serial.println(buttonPushCounter);

      Serial.write('\n');

      Serial.write('\r');

    }

    // Delay a little bit to avoid bouncing

    delay(50);

  }

  // save the current state as the last state, for next time through the loop

  lastButtonState = buttonState;

 

 

  if (buttonPushCounter % 4 == 0) {

    digitalWrite(ledPin, HIGH);

  } else {

    digitalWrite(ledPin, LOW);

  }

  Serial.flush();

  Serial.end();

  Serial.begin(9600);

  Serial.flush();

}

 

 

and i get something like this on serial:

 

on

number of button pushes = 1

on

number of button pushes = 2

on

number of button pushes = 3

on

number of button pushes = 4

on

number of button pushes = 5

 

etc.

 

and i want to get:

on

number of button pushes = 1 ----- and on this line 1 to be replaced with 2 at the next count, then with 3 and so on..

 

I have tryed Serial.print( '\r' )  for carryege return but didnt workt.

 

Can someone tell me where im wrong?? Or what i need to print so see what i want.

  • Sign in to reply
  • Cancel
Parents
  • RParkerE
    RParkerE over 9 years ago

    Another "workaround" would be to figure out how many lines long the Arduino Serial Monitor is when you are using it and feed it that many line feeds effectively clearing the screen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • RParkerE
    RParkerE over 9 years ago

    Another "workaround" would be to figure out how many lines long the Arduino Serial Monitor is when you are using it and feed it that many line feeds effectively clearing the screen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • roby1
    roby1 over 9 years ago in reply to RParkerE

    i know what u mean..i can use  ..."Serial.print()" and this will feed the screen with "empty" values so i will be able to see the " clear screen"...but thats not an option in my case....but thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to RParkerE

    Pter, I think that the Arduino Serial Monitor can't be managed in this way as this is - as a matter of fact - a java multi line text window that canbe resized as you want.

     

    What is needed is a terminal supporting ANSI Escapes, it is correct and in practice this means a terminal program (like the Linux term) that can be configured in VT100+ mode.

     

    Enrico