• Products and Partners
    Products and Partners
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
Member's Forum Arduino Serial
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 632 subscribers
  • Views 2368 views
  • Users 0 members are here
  • arduino serial stuff
Related

Arduino Serial

roby1
roby1 over 9 years ago

Hi..i have a question, maybe a noob one for ppl who know. I have maked a counter each time when i press the button the counter increments with 1 and display on serial something like:

nr = 1, nr = 2, nr = 3 ...etc. What i wanna know and i have tryed over 4 days is how i diplay only once the value on a single line and each time when i count,  ""to somehow overwrite"" the existing value and displayng it like: ""nr = 1"" then on the same line 1 is replaced with 2..then with 3 and so on every time i count.  More simple, then same line remains unchanged and only the value get overrited (upgraded).

 

HERE IS THE CODE:

 

const int  buttonPin = 2;    // the pin that the pushbutton is attached to

const int ledPin = 10;       // the pin that the LED is attached to

 

 

// Variables will change:

int buttonPushCounter = 0;   // counter for the number of button presses

int buttonState = 0;         // current state of the button

int lastButtonState = 0;     // previous state of the button

 

 

void setup()

{

  pinMode(buttonPin, INPUT);

  pinMode(ledPin, OUTPUT);

  Serial.begin(9600);

}

 

 

 

 

void loop()

{

  buttonState = digitalRead(buttonPin);

 

 

  if (buttonState != lastButtonState)

  {

    if (buttonState == HIGH)

    {

      buttonPushCounter++;

      Serial.println("on");

      Serial.print("number of button pushes: ");

      Serial.println(buttonPushCounter);

      Serial.write('\n');

      Serial.write('\r');

    }

    // Delay a little bit to avoid bouncing

    delay(50);

  }

  // save the current state as the last state, for next time through the loop

  lastButtonState = buttonState;

 

 

  if (buttonPushCounter % 4 == 0) {

    digitalWrite(ledPin, HIGH);

  } else {

    digitalWrite(ledPin, LOW);

  }

  Serial.flush();

  Serial.end();

  Serial.begin(9600);

  Serial.flush();

}

 

 

and i get something like this on serial:

 

on

number of button pushes = 1

on

number of button pushes = 2

on

number of button pushes = 3

on

number of button pushes = 4

on

number of button pushes = 5

 

etc.

 

and i want to get:

on

number of button pushes = 1 ----- and on this line 1 to be replaced with 2 at the next count, then with 3 and so on..

 

I have tryed Serial.print( '\r' )  for carryege return but didnt workt.

 

Can someone tell me where im wrong?? Or what i need to print so see what i want.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    Putty is a perfectly good example of a terminal and can respond to commands to change colour, move cursor etc etc, just look at the mirad of Raspberry PI scrips that make use of this

    Here is an example of one from a friend of mine that installs a whole bunch of stuff and heavily leverages terminal emulation escape sequences to make a much friendlier screen

     

    https://bitbucket.org/snippets/scargill/ekon6o/the-script

    I am pretty sure that by default putty will emulate an  XTerm screen https://www.x.org/docs/xterm/ctlseqs.pdf

     

    it certainly follows the ansi colour commands so for example, just put putty in  local echo and type "ESC"[0;92m and continue typing, The "ESC" is the actual escape key on the keyboard, the text will now be green

     

    oir this simple mod to the ASCIITabletest.ino example will glean a colourful output

     

     

    .......

    void loop() {

      // prints value unaltered, i.e. the raw binary version of the

      // byte. The serial monitor interprets all bytes as

      // ASCII, so 33, the first number,  will show up as '!'

      Serial.print("\x1B[0;");

      Serial.print(thisByte);

      Serial.print("m");

      Serial.write(thisByte);

     

     

      Serial.print(", dec: ");

      // prints value as string as an ASCII-encoded decimal (base 10).

      // Decimal is the  default format for Serial.print() and Serial.println(),

      // so no modifier is needed:

      Serial.print(thisByte);

    .......

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    Putty is a perfectly good example of a terminal and can respond to commands to change colour, move cursor etc etc, just look at the mirad of Raspberry PI scrips that make use of this

    Here is an example of one from a friend of mine that installs a whole bunch of stuff and heavily leverages terminal emulation escape sequences to make a much friendlier screen

     

    https://bitbucket.org/snippets/scargill/ekon6o/the-script

    I am pretty sure that by default putty will emulate an  XTerm screen https://www.x.org/docs/xterm/ctlseqs.pdf

     

    it certainly follows the ansi colour commands so for example, just put putty in  local echo and type "ESC"[0;92m and continue typing, The "ESC" is the actual escape key on the keyboard, the text will now be green

     

    oir this simple mod to the ASCIITabletest.ino example will glean a colourful output

     

     

    .......

    void loop() {

      // prints value unaltered, i.e. the raw binary version of the

      // byte. The serial monitor interprets all bytes as

      // ASCII, so 33, the first number,  will show up as '!'

      Serial.print("\x1B[0;");

      Serial.print(thisByte);

      Serial.print("m");

      Serial.write(thisByte);

     

     

      Serial.print(", dec: ");

      // prints value as string as an ASCII-encoded decimal (base 10).

      // Decimal is the  default format for Serial.print() and Serial.println(),

      // so no modifier is needed:

      Serial.print(thisByte);

    .......