Member's Forum Raspberry Pi I/O pins.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 631 subscribers
  • Views 1337 views
  • Users 0 members are here
Related

Raspberry Pi I/O pins.

DAB
DAB over 8 years ago

Hi all,

 

I was doing some testing yesterday and discovered that the I/O pins on the RPi come up with interesting voltages on powerup.

 

I had just assumed that they would all come up at ground state, but we measured several pins and found them at 0.7, 1.2, 1.7, and 2.7 volts output.

 

We were trying to debug a driver circuit I designed, but noticed the default was at 1.2 volts and thought we might have a defective board. So we installed a brand new RPi 3 and found the pins at the above stated levels.

 

I am VERY disappointed in the RPi designers for not defaulting the pins to ground state until they are accessed by software.

 

Hopefully, they will correct this oversight in the next version.

 

Having random output levels could really do some damage to external circuits wired into an RPi.

 

DAB

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 8 years ago

    I personally would expect high impedance as preferable to prevent any risk of damage (e.g. shorting). If the line must be low or high when not driven by the MCU, then an external pull-up or pull-down resistor should do the trick. I suspect some of the voltages you see might be stray voltages capacitively coupled due to the close trace/pin spacing and high impedance of the meter. If not, and lines are driven with strange voltages, that would be rather surprising but may be able to be worked around.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 8 years ago

    I personally would expect high impedance as preferable to prevent any risk of damage (e.g. shorting). If the line must be low or high when not driven by the MCU, then an external pull-up or pull-down resistor should do the trick. I suspect some of the voltages you see might be stray voltages capacitively coupled due to the close trace/pin spacing and high impedance of the meter. If not, and lines are driven with strange voltages, that would be rather surprising but may be able to be worked around.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • DAB
    DAB over 8 years ago in reply to Gough Lui

    That was my initial thought, but we were trying to drive the pin low across a transistor base connection.

    Even at high impedance, you expect the output to be 0 volts with the pin set to a logic zero.

     

    DAB