Member's Forum Raspberry Pi I/O pins.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 631 subscribers
  • Views 1346 views
  • Users 0 members are here
Related

Raspberry Pi I/O pins.

DAB
DAB over 8 years ago

Hi all,

 

I was doing some testing yesterday and discovered that the I/O pins on the RPi come up with interesting voltages on powerup.

 

I had just assumed that they would all come up at ground state, but we measured several pins and found them at 0.7, 1.2, 1.7, and 2.7 volts output.

 

We were trying to debug a driver circuit I designed, but noticed the default was at 1.2 volts and thought we might have a defective board. So we installed a brand new RPi 3 and found the pins at the above stated levels.

 

I am VERY disappointed in the RPi designers for not defaulting the pins to ground state until they are accessed by software.

 

Hopefully, they will correct this oversight in the next version.

 

Having random output levels could really do some damage to external circuits wired into an RPi.

 

DAB

  • Sign in to reply
  • Cancel
Parents
  • jomoenginer
    jomoenginer over 8 years ago

    I believe the issue is how the gpio pins on the Raspberry Pi  are set at boot.   You could write a script that ran at boot that changes the states so they are the same.  There might be a better way but you would want to be cautious that you don't affect any of the on board devices.

     

    You can view the states of the GPIO pins on your RasPi by running 'gpio readall'

     

    Ex:

    $ gpio readall
    linedata: processor : 0
    
    
    linedata: model name : ARMv6-compatible processor rev 7 (v6l)
    
    
    linedata: BogoMIPS : 697.95
    
    
    linedata: Features : half thumb fastmult vfp edsp java tls 
    
    
    linedata: CPU implementer : 0x41
    
    
    linedata: CPU architecture: 7
    
    
    linedata: CPU variant : 0x0
    
    
    linedata: CPU part : 0xb76
    
    
    linedata: CPU revision : 7
    
    
    linedata: 
    
    
    linedata: Hardware : BCM2835
    
    
    linedata: Revision : 0010
    
    
    Revision got: Revision : 0010
    
    
     +-----+-----+---------+------+---+--B Plus--+---+------+---------+-----+-----+
     | BCM | wPi |   Name  | Mode | V | Physical | V | Mode | Name    | wPi | BCM |
     +-----+-----+---------+------+---+----++----+---+------+---------+-----+-----+
     |     |     |    3.3v |      |   |  1 || 2  |   |      | 5v      |     |     |
     |   2 |   8 |   SDA.1 | ALT0 | 1 |  3 || 4  |   |      | 5V      |     |     |
     |   3 |   9 |   SCL.1 | ALT0 | 1 |  5 || 6  |   |      | 0v      |     |     |
     |   4 |   7 | GPIO. 7 |   IN | 1 |  7 || 8  | 1 | ALT0 | TxD     | 15  | 14  |
     |     |     |      0v |      |   |  9 || 10 | 1 | ALT0 | RxD     | 16  | 15  |
     |  17 |   0 | GPIO. 0 |   IN | 0 | 11 || 12 | 0 | IN   | GPIO. 1 | 1   | 18  |
     |  27 |   2 | GPIO. 2 |   IN | 0 | 13 || 14 |   |      | 0v      |     |     |
     |  22 |   3 | GPIO. 3 |   IN | 0 | 15 || 16 | 0 | IN   | GPIO. 4 | 4   | 23  |
     |     |     |    3.3v |      |   | 17 || 18 | 0 | IN   | GPIO. 5 | 5   | 24  |
     |  10 |  12 |    MOSI | ALT0 | 0 | 19 || 20 |   |      | 0v      |     |     |
     |   9 |  13 |    MISO | ALT0 | 0 | 21 || 22 | 1 | IN   | GPIO. 6 | 6   | 25  |
     |  11 |  14 |    SCLK | ALT0 | 0 | 23 || 24 | 1 | OUT  | CE0     | 10  | 8   |
     |     |     |      0v |      |   | 25 || 26 | 1 | OUT  | CE1     | 11  | 7   |
     |   0 |  30 |   SDA.0 |   IN | 1 | 27 || 28 | 1 | IN   | SCL.0   | 31  | 1   |
     |   5 |  21 | GPIO.21 |   IN | 1 | 29 || 30 |   |      | 0v      |     |     |
     |   6 |  22 | GPIO.22 |   IN | 1 | 31 || 32 | 0 | IN   | GPIO.26 | 26  | 12  |
     |  13 |  23 | GPIO.23 |   IN | 0 | 33 || 34 |   |      | 0v      |     |     |
     |  19 |  24 | GPIO.24 |   IN | 0 | 35 || 36 | 1 | OUT  | GPIO.27 | 27  | 16  |
     |  26 |  25 | GPIO.25 |   IN | 0 | 37 || 38 | 0 | IN   | GPIO.28 | 28  | 20  |
     |     |     |      0v |      |   | 39 || 40 | 0 | IN   | GPIO.29 | 29  | 21  |
     +-----+-----+---------+------+---+----++----+---+------+---------+-----+-----+
     | BCM | wPi |   Name  | Mode | V | Physical | V | Mode | Name    | wPi | BCM |
     +-----+-----+---------+------+---+--B Plus--+---+------+---------+-----+-----+

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 8 years ago in reply to jomoenginer

    We had the pin set to low, but I still saw about 1.1v drop across my transistor driver from the base to the emitter.

     

    I was expecting there to be no voltage across the junction with the base at ground level.

     

    If you cannot expect the I/O pin to be grounded under that kind of small load, then something is very wrong with their design.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 8 years ago in reply to jomoenginer

    We had the pin set to low, but I still saw about 1.1v drop across my transistor driver from the base to the emitter.

     

    I was expecting there to be no voltage across the junction with the base at ground level.

     

    If you cannot expect the I/O pin to be grounded under that kind of small load, then something is very wrong with their design.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jomoenginer
    jomoenginer over 8 years ago in reply to DAB

    Well, low does not necessarily mean off.  A low could mean just low current or low voltage such as 1.1v as you had experienced. You might want to contact the Raspberry Pi folks to see if it is possible to completely disable the pin you are working with.