• Products and Partners
    Products and Partners
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
Member's Forum Understanding the behaviour of a 4026BE Decade Counter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 630 subscribers
  • Views 1833 views
  • Users 0 members are here
  • 4026be
  • decade counter
Related

Understanding the behaviour of a 4026BE Decade Counter

Andrew J
Andrew J over 7 years ago

I have a very simple circuit (see below), basically a 4026BE Decade Counter linked to a 7-Seg display; when I press a momentary button to apply +ve power to the counter pin (1) it increases the 'score' on the LED by 1.  No inputs are floating, I've debounced the button and it all works fine, except....

If I power it via a 9V source, either a 9V battery or a 9V adapter, the LED displays 0 (zero) when I first apply the power (momentary switch is up); pressing the switch increments by 1.  Jobs a good 'un as they say and it's exactly how I want it to be.

If I power it via a 5V regulated source - i.e. the 9V source connected to a LM7805 and its 5V output routed to the momentary switch (up) the LED displays '9' usually, sometimes random segments, when I first apply the power.  Pressing the button increments by 1 and it all works fine. 

The counter pin is pulled low with a resistor/capacitor combination (pulls it low and debounces the button) and I've measured 0V at that pin at power on.  Reset pin is pulled low as well. 

 

I'm looking for some insights in why this might be happening: why might a lower voltage be causing output on some pins of the 4026B?  Could it be because the Display Enable pin is permanently connected to source, thus 9V or 5V?  I could power the circuit via 9V and be done, or use 5V and just press the reset button to set to 0, but I think I'll be missing a learning opportunity here (I'm very new to electronics.)  Also, the rest of what I'm building will require 5V so I thought I'd try and keep it the same. 

 

image

 

Thanks,

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 7 years ago

    Generally, as far as I'm aware, there's no guaranteed power-on state for such a counter? The difference may just boil down to an internal race condition with the IC's internal transistors - different voltages will change their behaviour.

     

    I think it might be possible to have the reset line held low long enough post-power-up to allow for it to start at zero if you use a capacitor and/or resistor combination although I've never tried this myself.

     

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to Gough Lui

    Thanks for your input guys.  Gough: putting a capacitor (only 0.1 uF) linking pin 16 and pin 15 brings up 15 just long enough to keep the counter stable and it initialises to zero.  Just what I was looking for.

     

    Cheers

     

    Andrew

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to Andrew J

    Hi Andrew;

     

    If you haven't already done it you might try a .01 uF between the Pin 16 and Pin 2. This is called a decoupling capacitor and it can stabilize the voltage and help with this type of problem sometimes.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    Sometimes the only fix is to do a bunch of empirical experimenting like you have done and hopefully get the right combination.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to jw0752

    Hi John,

     

    I tried that with no change: the LED still showed 9 at power on.  Also, with the capacitor between pin 16 and -ve (effectively the same.)  However, it did prompt me to go back to my text to read about decoupling capacitors to find that it only talked about coupling capacitors!  One quick Google later and I see what you are saying, so thanks for chipping in. 

     

    I also tried with a 0.01uF and 100uF capacitor in parallel to the circuit but that didn't help either.  Putting a 0.1uF capacitor between pin 16 (+ve) and pin 15 (reset) to temporarily pull 15 up keeps the LED at zero and allows the button to increment the count (and the reset button to reset to zero.)  Interestingly, a 0.01uF capacitor, at the same position, kept the LED at zero but didn't allow incrementing with the button press: it must be sinking the +ve pulse faster than the chip can recognise it - although the capacitor should be charged by that point so I'm not sure really.

     

    Thanks

     

    Andrew

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 7 years ago in reply to jw0752

    Hi John,

     

    I tried that with no change: the LED still showed 9 at power on.  Also, with the capacitor between pin 16 and -ve (effectively the same.)  However, it did prompt me to go back to my text to read about decoupling capacitors to find that it only talked about coupling capacitors!  One quick Google later and I see what you are saying, so thanks for chipping in. 

     

    I also tried with a 0.01uF and 100uF capacitor in parallel to the circuit but that didn't help either.  Putting a 0.1uF capacitor between pin 16 (+ve) and pin 15 (reset) to temporarily pull 15 up keeps the LED at zero and allows the button to increment the count (and the reset button to reset to zero.)  Interestingly, a 0.01uF capacitor, at the same position, kept the LED at zero but didn't allow incrementing with the button press: it must be sinking the +ve pulse faster than the chip can recognise it - although the capacitor should be charged by that point so I'm not sure really.

     

    Thanks

     

    Andrew

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    Sometimes the only fix is to do a bunch of empirical experimenting like you have done and hopefully get the right combination.

     

    John